![]() |
SDL API Guide for J721S2
|
This structure contains the different configuration used for PBIST test of ROM.
Design: PROC_SDL-6145
Data Fields | |
uint32_t | D |
uint32_t | E |
uint32_t | CA2 |
uint32_t | CL0 |
uint32_t | CA3 |
uint32_t | I0 |
uint32_t | CL1 |
uint32_t | I3 |
uint32_t | I2 |
uint32_t | CL2 |
uint32_t | CA1 |
uint32_t | CA0 |
uint32_t | CL3 |
uint32_t | I1 |
uint32_t | RAMT |
uint32_t | CSR |
uint32_t | CMS |
uint32_t SDL_PBIST_romTest::D |
ROM test value for D Value for the PBIST Test of ROM Vector D
uint32_t SDL_PBIST_romTest::E |
ROM test value for E Value for the PBIST Test of ROM Vector E
uint32_t SDL_PBIST_romTest::CA2 |
ROM test value for CA2 Value for the PBIST Test of ROM Vector CA2
uint32_t SDL_PBIST_romTest::CL0 |
ROM test value for CL0 Value for the PBIST Test of ROM Vector CL0
uint32_t SDL_PBIST_romTest::CA3 |
ROM test value for CA3 Value for the PBIST Test of ROM Vector CA3
uint32_t SDL_PBIST_romTest::I0 |
ROM test value for I0 Value for the PBIST Test of ROM Vector I0
uint32_t SDL_PBIST_romTest::CL1 |
ROM test value for CL1 Value for the PBIST Test of ROM Vector CL1
uint32_t SDL_PBIST_romTest::I3 |
ROM test value for I3 Value for the PBIST Test of ROM Vector I3
uint32_t SDL_PBIST_romTest::I2 |
ROM test value for I2 Value for the PBIST Test of ROM Vector I2
uint32_t SDL_PBIST_romTest::CL2 |
ROM test value for CL2 Value for the PBIST Test of ROM Vector CL2
uint32_t SDL_PBIST_romTest::CA1 |
ROM test value for CA1 Value for the PBIST Test of ROM Vector CA1
uint32_t SDL_PBIST_romTest::CA0 |
ROM test value for CA0 Value for the PBIST Test of ROM Vector CA0
uint32_t SDL_PBIST_romTest::CL3 |
ROM test value for CL3 Value for the PBIST Test of ROM Vector CL3
uint32_t SDL_PBIST_romTest::I1 |
ROM test value for I1 Value for the PBIST Test of ROM Vector I1
uint32_t SDL_PBIST_romTest::RAMT |
ROM test value for RAMT Value for the PBIST Test of ROM Vector RAMT
uint32_t SDL_PBIST_romTest::CSR |
ROM test value for CSR Value for PBIST Test of ROM Vector CSR
uint32_t SDL_PBIST_romTest::CMS |
ROM test value for CMS Value for the PBIST Test Of ROM Vector CMS