49 #if defined (SOC_J7200) 50 #include <src/ip/sdl_ip_mtog.h> 51 #include <src/ip/sdlr_mtog.h> 52 #include <src/sdl/tog/soc/j7200/sdl_soc_mtog.h> 55 #if defined (SOC_J721S2) 56 #include <src/ip/sdl_ip_mtog.h> 57 #include <src/ip/sdlr_mtog.h> 61 #if defined (SOC_J784S4) 62 #include <src/ip/sdl_ip_mtog.h> 63 #include <src/ip/sdlr_mtog.h> 64 #include <src/sdl/tog/soc/j784s4/sdl_soc_mtog.h> 68 #define SDL_MTOG_FORCE_KEY ((uint32_t) 0x95U) uint8_t SDL_MTOG_Inst
Definition: sdl_soc_mtog.h:59
Definition: sdl_mtog.h:132
Master TOG Static Registers.
Definition: sdl_mtog.h:125
int32_t SDL_MTOG_getStaticRegisters(SDL_MTOG_Inst instance, SDL_MTOG_staticRegs *pStaticRegs)
Readback Static configuration register.
uint32_t SDL_MTOGVal
Definition: sdl_ip_mtog.h:83
int32_t SDL_MTOG_verifyConfig(SDL_MTOG_Inst instance, const SDL_MTOG_config *pConfig)
Verifying written configuration with Master TOG module.
int32_t SDL_MTOG_init(SDL_MTOG_Inst instance, const SDL_MTOG_config *pConfig)
Initialize Master TOG module with respect of instance.
int32_t SDL_MTOG_forceTimeout(SDL_MTOG_Inst instance)
Force a timeout.
int32_t SDL_MTOG_stop(SDL_MTOG_Inst instance)
Stop the timeout function.
int32_t SDL_MTOG_start(SDL_MTOG_Inst instance)
Start the timeout function.
SDL_MTOGVal timeOut
Definition: sdl_mtog.h:134
int32_t SDL_MTOG_reset(SDL_MTOG_Inst instance)
Reset the timeout functionality.
uint32_t mtogCtrlRegister
Definition: sdl_mtog.h:127