![]() |
SDL API Guide for J721S2
|
Header file containing various enumerations, structure definitions and function.
(C) Copyright 2021, Texas Instruments, Inc.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Go to the source code of this file.
Data Structures | |
struct | SDL_PMU_staticRegs |
PMU Static Registers structure. More... | |
Macros | |
#define | SDL_ARM_R5_PMU_CYCLE_COUNTER_NUM (31U) |
#define | SDL_ARM_R5_PMU_CFG_CNTR_EVENT_TYPE_MASK (0x000000FFU) |
#define | SDL_ARM_R5_PMU_CFG_CNTR_EVENT_TYPE_SHIFT (0x00000000U) |
#define | SDL_ARM_R5_PMU_CFG_CNTR_EVENT_TYPE_RESETVAL (0x00000000U) |
#define | SDL_ARM_R5_PMU_CFG_CNTR_EVENT_TYPE_MAX (0x000000FFU) |
Functions | |
void | SDL_R5PMU_cfg (uint32_t cycleCntDiv, uint32_t exportEvents, uint32_t userEnable) |
Configure the Performance Management Unit (PMU) More... | |
int32_t | SDL_R5PMU_verifyCfg (uint32_t cycleCntDiv, uint32_t exportEvents) |
Configure the Performance Management Unit (PMU) More... | |
void | SDL_R5PMU_enableAllCntrs (uint32_t enable) |
Enable/disable all PMU counters. More... | |
uint32_t | SDL_R5PMU_getNumCntrs (void) |
Get the number of PMU counters supported. More... | |
void | SDL_R5PMU_cfgCntr (uint32_t cntrNum, SDL_R5PmuEventType eventType) |
Configure a PMU counter. More... | |
void | SDL_R5PMU_enableCntrOverflowIntr (uint32_t cntrNum, uint32_t enable) |
Enable/disable overflow interrupt generation for a PMU counter. More... | |
void | SDL_R5PMU_enableCntr (uint32_t cntrNum, uint32_t enable) |
Enable/disable a PMU counter. More... | |
uint32_t | SDL_R5PMU_readCntr (uint32_t cntrNum) |
Read a PMU counter. More... | |
void | SDL_R5PMU_setResetCntr (uint32_t cntrNum, uint32_t cntrVal) |
Set a PMU counter. More... | |
uint32_t | SDL_R5PMU_readCntrOverflowStatus (void) |
Read the overflow status for all of the counters. More... | |
void | SDL_R5PMU_clearCntrOverflowStatus (uint32_t cntrMask) |
Clear the overflow flag for the specified counter(s) More... | |
void | SDL_R5PMU_resetCycleCnt (void) |
Reset the cycle counter to zero. More... | |
void | SDL_R5PMU_resetCntrs (void) |
Reset all counters to zero. More... | |
void | SDL_R5PMU_readStaticRegisters (SDL_PMU_staticRegs *pStaticRegs) |
PMU API to Read the Static Registers. This function reads the values of the static registers such as cycleCntDiv, exportEvents and userEnable status. More... | |