![]() |
SDL API Guide for J721S2
|
Functions | |
int32_t | SDL_pokSetControl (SDL_wkupCtrlRegsBase_t *pBaseAddress, const SDL_POK_config *pPokCfg, SDL_POK_Inst instance) |
write the POK configuration for the specified POK control register More... | |
int32_t | SDL_pokGetControl (SDL_wkupCtrlRegsBase_t *pBaseAddress, const SDL_POK_config *pPokCfg, SDL_pokVal_t *pPokVal, SDL_POK_Inst instance) |
Read the POK configuration for the specified POK control register. More... | |
int32_t | SDL_porSetControl (SDL_wkupCtrlRegsBase_t *pBaseAddress, const SDL_pokPorCfg_t *pPorCfg) |
write the POR configuration for the specified POK control register More... | |
int32_t SDL_pokSetControl | ( | SDL_wkupCtrlRegsBase_t * | pBaseAddress, |
const SDL_POK_config * | pPokCfg, | ||
SDL_POK_Inst | instance | ||
) |
write the POK configuration for the specified POK control register
This API supports the enable/disable of the POK hysterisis and Voltage Detection for a given POK control register
pBaseAddress | [IN] Pointer to the Wakeup Control Register |
pPokCfg | [IN] Pointer to the POK control register to be written |
instance | [IN] POK ID of which POK to be updated |
int32_t SDL_pokGetControl | ( | SDL_wkupCtrlRegsBase_t * | pBaseAddress, |
const SDL_POK_config * | pPokCfg, | ||
SDL_pokVal_t * | pPokVal, | ||
SDL_POK_Inst | instance | ||
) |
Read the POK configuration for the specified POK control register.
This API supports the enable/disable of the POK hysterisis and Voltage Detection for a given POK control register
pBaseAddress | [IN] Pointer to the Wakeup Control Register |
pPokCfg | [IN] Pointer to the POK control register values to be read |
pPokVal | [OUT] Pointer to the POK control register to be read |
instance | [IN] POK ID of which POK to be updated |
int32_t SDL_porSetControl | ( | SDL_wkupCtrlRegsBase_t * | pBaseAddress, |
const SDL_pokPorCfg_t * | pPorCfg | ||
) |
write the POR configuration for the specified POK control register
This API supports the enable/disable of the POK hysterisis and Voltage Detection for a given POK control register
pBaseAddress | [IN] Pointer to the Wakeup Control Register |
pPorCfg | [IN] Pointer to the POR configuration |