![]() |
SDL API Guide for J721S2
|
Functions | |
int32_t | SDL_LBIST_enableIsolation (SDL_lbistRegs *pLBISTRegs) |
Enable LBIST Isolation. More... | |
int32_t | SDL_LBIST_disableIsolation (SDL_lbistRegs *pLBISTRegs) |
Disable LBIST Isolation. More... | |
int32_t | SDL_LBIST_reset (SDL_lbistRegs *pLBISTRegs) |
Reset LBIST. More... | |
int32_t | SDL_LBIST_enableRunBISTMode (SDL_lbistRegs *pLBISTRegs) |
Enable run BIST mode. More... | |
int32_t | SDL_LBIST_clearRunBISTMode (SDL_lbistRegs *pLBISTRegs) |
Clear run BIST mode. More... | |
int32_t | SDL_LBIST_start (SDL_lbistRegs *pLBISTRegs) |
LBIST start. More... | |
int32_t | SDL_LBIST_stop (SDL_lbistRegs *pLBISTRegs) |
LBIST stop. More... | |
int32_t | SDL_LBIST_isRunning (const SDL_lbistRegs *pLBISTRegs, bool *pIsRunning) |
LBIST check running. More... | |
int32_t | SDL_LBIST_isDone (const SDL_lbistRegs *pLBISTRegs, bool *pIsDone) |
LBIST check done. More... | |
int32_t | SDL_LBIST_programConfig (SDL_lbistRegs *pLBISTRegs, const SDL_LBIST_config_t *pConfig) |
LBIST Program config. More... | |
int32_t | SDL_LBIST_getMISR (SDL_lbistRegs *pLBISTRegs, uint32_t *pMISRValue) |
LBIST get MISR. More... | |
int32_t | SDL_LBIST_getExpectedMISR (const uint32_t *pLBISTSig, uint32_t *pExpectedMISRValue) |
LBIST get expected MISR. More... | |
int32_t SDL_LBIST_enableIsolation | ( | SDL_lbistRegs * | pLBISTRegs | ) |
Enable LBIST Isolation.
This function enables LBIST isolation. Isolation needs to be enabled before. starting LBIST.
pLBISTRegs | [IN] Pointer to LBIST register map |
int32_t SDL_LBIST_disableIsolation | ( | SDL_lbistRegs * | pLBISTRegs | ) |
Disable LBIST Isolation.
This function disables LBIST isolation. This is done after LBIST is complete. NOTE: This should not be called when the LBIST test is running. If called while LBIST test is running, it may lead to undefined behaviour.
pLBISTRegs | [IN] Pointer to LBIST register map |
int32_t SDL_LBIST_reset | ( | SDL_lbistRegs * | pLBISTRegs | ) |
Reset LBIST.
This function resets LBIST module. This is done preparing for a new LBIST execution, as well as exiting an LBIST execution.
pLBISTRegs | [IN] Pointer to LBIST register map |
int32_t SDL_LBIST_enableRunBISTMode | ( | SDL_lbistRegs * | pLBISTRegs | ) |
Enable run BIST mode.
This function enables Run BIST mode. This is needed to be set before starting LBIST.
pLBISTRegs | [IN] Pointer to LBIST register map |
int32_t SDL_LBIST_clearRunBISTMode | ( | SDL_lbistRegs * | pLBISTRegs | ) |
Clear run BIST mode.
This function clears Run BIST mode. This is done after LBIST execution is complete. If called in the middle of the test, the test may terminate prematurely.
pLBISTRegs | [IN] Pointer to LBIST register map |
int32_t SDL_LBIST_start | ( | SDL_lbistRegs * | pLBISTRegs | ) |
LBIST start.
This function starts LBIST execution.
pLBISTRegs | [IN] Pointer to LBIST register map |
int32_t SDL_LBIST_stop | ( | SDL_lbistRegs * | pLBISTRegs | ) |
LBIST stop.
This function stops LBIST execution. This is normally called after checking the signature and clearing the run-BIST mode. But this can also be called asynchronously to stop LBIST in the middle of a test.
pLBISTRegs | [IN] Pointer to LBIST register map |
int32_t SDL_LBIST_isRunning | ( | const SDL_lbistRegs * | pLBISTRegs, |
bool * | pIsRunning | ||
) |
LBIST check running.
This function checks if LBIST is running. Note that this is specifically checking if the LBIST is currently running, and this is different from done status.
pLBISTRegs | [IN] Pointer to LBIST register map |
pIsRunning | [OUT] Pointer to variable to indicate running status SDL_TRUE : LBIST is running SDL_FALSE: LBIST is not running |
int32_t SDL_LBIST_isDone | ( | const SDL_lbistRegs * | pLBISTRegs, |
bool * | pIsDone | ||
) |
LBIST check done.
This function checks if LBIST is complete. Note that this is different from running status, which shows if the LBIST is curently running.
pLBISTRegs | [IN] Pointer to LBIST register map |
pIsDone | [OUT] Pointer to variable to indicate done status SDL_TRUE : LBIST is done SDL_FALSE: LBIST is not complete |
int32_t SDL_LBIST_programConfig | ( | SDL_lbistRegs * | pLBISTRegs, |
const SDL_LBIST_config_t * | pConfig | ||
) |
LBIST Program config.
This function configures the parameters for LBIST execution.
pLBISTRegs | [IN] Pointer to LBIST register map |
pConfig | [IN] Pointer to LBIST program configuration |
int32_t SDL_LBIST_getMISR | ( | SDL_lbistRegs * | pLBISTRegs, |
uint32_t * | pMISRValue | ||
) |
LBIST get MISR.
This function returns the MISR register. This register holds the Multiple Input Signature generated by LBIST test. It should be called after the LBIST execution has completed.
pLBISTRegs | [IN] Pointer to LBIST register map |
pMISRValue | [OUT] Pointer to MISR value return |
int32_t SDL_LBIST_getExpectedMISR | ( | const uint32_t * | pLBISTSig, |
uint32_t * | pExpectedMISRValue | ||
) |
LBIST get expected MISR.
This function returns the expected MISR register value. This register holds the expected Multiple Input Signature generated by LBIST test.
pLBISTSig | [IN] Pointer to LBIST Sig Register |
pExpectedMISRValue | [OUT] Pointer to MISR value return |