![]() |
SDL API Guide for J721S2
|
Functions | |
void | SDL_R5MPU_Enable (uint32_t enable) |
Enable/disable the Memory Protection Unit (MPU) More... | |
uint32_t | SDL_R5MPU_getNumRegions (void) |
Get the number of unified MPU regions supported. More... | |
void | SDL_R5MPU_Cfg (uint32_t regionNum, uint32_t baseAddrRegVal, uint32_t sizeRegVal, uint32_t accessCtrlRegVal) |
Configure an MPU region. More... | |
int32_t | SDL_R5MPU_VerifyCfg (uint32_t regionNum, uint32_t baseAddrRegVal, uint32_t sizeRegVal, uint32_t accessCtrlRegVal) |
Verify an MPU region that is previously configured. More... | |
void | SDL_R5FMPU_enableRegion (uint32_t regionNum, uint32_t enable) |
Enable/disable an MPU region. More... | |
int32_t | SDL_R5MPU_VerifyEnableRegion (uint32_t regionNum, uint32_t enable) |
Verifies the previously called Enable/disable an MPU region API. More... | |
void | SDL_R5MPU_readStaticRegisters (SDL_MPU_staticRegs *pStaticRegs, uint32_t regionNum) |
MPU API to Read the Static Registers. This function reads the values of the static registers such as System Control Register, MPU Type Register and MPU Region Number Register. More... | |
void SDL_R5MPU_Enable | ( | uint32_t | enable | ) |
Enable/disable the Memory Protection Unit (MPU)
This function is used to enable or disable the MPU.
enable | [IN] 0=MPU is disabled, otherwise MPU is enabled |
uint32_t SDL_R5MPU_getNumRegions | ( | void | ) |
Get the number of unified MPU regions supported.
This function is used to get the number of unified MPU regions supported.
void SDL_R5MPU_Cfg | ( | uint32_t | regionNum, |
uint32_t | baseAddrRegVal, | ||
uint32_t | sizeRegVal, | ||
uint32_t | accessCtrlRegVal | ||
) |
Configure an MPU region.
This function is used to configure an MPU region.
The value arguments provided to this function are directly written into the corresponding R5 system register. As a result, the values must be constructed per the expected register format.
See the "MPU memory region programming registers" section of the ARM Cortex R5 TRM for more information.
regionNum | [IN] Region number |
baseAddrRegVal | [IN] Value written to the MPU Region Base Address Register |
sizeRegVal | [IN] Value written to the MPU Size and Enable Register |
accessCtrlRegVal | [IN] Value written to the MPU Region Access Control Register |
int32_t SDL_R5MPU_VerifyCfg | ( | uint32_t | regionNum, |
uint32_t | baseAddrRegVal, | ||
uint32_t | sizeRegVal, | ||
uint32_t | accessCtrlRegVal | ||
) |
Verify an MPU region that is previously configured.
This function is used to verify the previous configure an MPU region API.
The value arguments provided to this function are directly verfied against the corresponding R5 system register. As a result, the values must be constructed per the expected register format.
See the "MPU memory region programming registers" section of the ARM Cortex R5 TRM for more information.
regionNum | [IN] Region number |
baseAddrRegVal | [IN] Value written to the MPU Region Base Address Register |
sizeRegVal | [IN] Value written to the MPU Size and Enable Register |
accessCtrlRegVal | [IN] Value written to the MPU Region Access Control Register |
void SDL_R5FMPU_enableRegion | ( | uint32_t | regionNum, |
uint32_t | enable | ||
) |
Enable/disable an MPU region.
This function is used to enable or disable an MPU region.
regionNum | [IN] Region number |
enable | [IN] 0=The specified MPU region is disabled, otherwise it is enabled |
int32_t SDL_R5MPU_VerifyEnableRegion | ( | uint32_t | regionNum, |
uint32_t | enable | ||
) |
Verifies the previously called Enable/disable an MPU region API.
This function is used to verify enable or disable an MPU region.
regionNum | [IN] Region number |
enable | [IN] 0=The specified MPU region is disabled, otherwise it is enabled |
void SDL_R5MPU_readStaticRegisters | ( | SDL_MPU_staticRegs * | pStaticRegs, |
uint32_t | regionNum | ||
) |
MPU API to Read the Static Registers. This function reads the values of the static registers such as System Control Register, MPU Type Register and MPU Region Number Register.
pStaticRegs | [IN] Pointer to the static registers structure |
regionNum | [IN] Region number |