5.11. Release notes - 08_00_03 (EARLY ADOPTER RELEASE: 2)¶
Important
A Linux cold boot after a power-on does not fully boot MCU2_0 firmware. A warm “reboot” is required before running applications. To do this, type “reboot” on the linux prompt after login:
root@j721s2-evm:~# reboot
5.11.1. Features¶
Note
bold sections are not yet functional or tested, as indicated in each section.
5.11.1.1. Hardware support¶
J721S2 Alpha EVM support with Leo and Hera PMIC processor board
J721S2 ES1.0 support
Fusion1 RevC daughter card with UB960 FPDLink deserializer
IMX390 2MP CSI2 image sensor + UB953 FPDLink serializer
AR0233 2.5MP CSI2 image sensor + UB953 FPDLink serializer
AR0820 8MP CSI2 image sensor + UB953 FPDLink serializer
GESI(Gateway/Ethernet Switch/Industrial) daughter card (for additional ethernet and CAN ports)
Infotainment daughter card (for HDMI output)
5.11.1.2. Software features¶
Important
Below is a summary of key features. Refer individual SDK Components release notes for more details
5.11.1.2.1. Vision Apps (ADAS, Vision, DL demos)¶
Note
None of the demos listed in this section are able to run yet due to pending dependencies on Display drivers.
OpenVX based demos for ADAS, Vision, deep learning applications
FreeRTOS on C7x, R5F and Linux on A72
Integrates all major PSDK RTOS and PSDK LINUX SW components like TIDL, MMALIB, PDK, OpenVX, OpenGL, C7x algorithms, imaging/sensors, IPC, Linux, FreeRTOS, SPL/uboot.
Integrates all major HW components like CSI2 camera, eDP/HDMI display, UART, I2C, ethernet, SD card
Deep Learning demos
Image Classification demo
File based
Camera based
Standalone Semantic Segmentation application
File based
Camera based
Standalone Object Detection application
File based
Camera based
Auto valet parking (AVP) demo
semantic segmentation, Parking spot detect and Vehicle detect algorithms
1 channel, 3 algo mode (AVP1 demo)
3 channel, 3 algo mode - combined network for parking spot and vehicle detect (AVP2 demo)
3 channel, 5 algo mode - combined network for parking spot and vehicle detect + Three task network for Semantic Segmentation, Motion Segmentation and Depth Estimation (AVP3 demo)
DKAZE-based Visual Localization application
Debug support for the ability to debug intermediate layer information from TIDL node
Surround view demos
3D surround view using GPU on 4x 2MP 30fps live camera input
3D surround view calibration application
3D Surround view + AVP2 demo running simultaneously
3D surround view using GPU on 4x2MP 30fps live camera input
3 channel, 3 algo mode - combined network for parking spot and vehicle detect (AVP2 demo)
ADAS/Vision demos
Dense optical flow (DOF) demo
Stereo disparity engine demo
Single and multi camera to display (CSI2RX + VISS + LDC + MSC + Display) demo
C7x algorithm offload demo (with DMA acceleration)
Perception Toolkit (PTK) Demos
Camera based SFM and occupancy grid mapping using Dense optical flow HW engine
Radar and lidar occupancy grid mapping
Camera SFM, radar, lidar fusion for occupancy grid mapping
CV Demos
Structure from motion
OpenVX target nodes
image pre-processing (YUV 2 RGB) nodes for DL demos
image post-processing and visualization nodes for deep learning, DOF, Stereo demos
lidar, radar, camera SFM nodes for PTK demos
OpenGL nodes for surround view
Profiling, logging and other utility APIs
All included MCU tasks are split between MCU2_0 (VPAC HWA) and MCU2_1 (DMPAC HWA), leaving MCU3_0 and MCU3_1 free on main island
5.11.1.2.2. Platform Development Kit (PDK)¶
RTOS device drivers running on R5F, C7x, A72
Supported drivers and modules
Board diagnostic library
ENET CPSW (2G) in MCU and Main domains, RGMII, lwIP
CSL-FL (Chip support library)
IPC (inter processor communication)
MMCSD with FATFS
OSAL
SBL secondary bootloader (with DDR)
SCI Client (DMSC interface)
SPI driver (SPI, OSPI)
OSPI (NOR, NAND)
UART
UDMA and DRU
VPAC and DMAC (VHWA)
CSI-Rx
CSI-Tx
ECC
VIM
FreeRTOS Support on R5, C7x
Following is not yet functional in this release:
VISS -> MSC Flex-connect
DSS
Refer to PDK release notes LINK for more details.
5.11.1.2.3. MCU Software (MCUSW)¶
AutoSAR 4.3.1 MCAL driver and MCU1_0 example applications running on R5F (TI Arm Clang Compiler).
AutoSAR MCAL driver for Adc, Can, CDD IPC, Dio, Eth, Gpt, Pwm, Epwm Spi, Icu & Wdg
MCUSW ”boot app”
5.11.1.2.4. TI Deep learning Product (TIDL) and MMALIB¶
Port from J721E to J721S2 with reduced MSMC (4MB)
CNN Network performance improvement with update C7x/MMA features 10% to 25%
Support of PSAT and RELU6 activation functions
Updated MMALIB with exercising MMA REV2 IP enhancement features
Following is not yet functional in this release:
Support Tensor flow lite pre-quantized models with asymmetric quantization support
5.11.1.2.5. TI OpenVX (TIOVX)¶
OpenVX v1.1 compliant implementation with graph pipelining and user data object extension support
OpenVX API on A72 running Linux
OpenVX target kernels on C7x, R5F, A72
OpenVX v1.1 C6x optimized kernels recompiled for C7x
OpenVX nodes for
TIDL (C7x-MMA)
VISS (R5F)
LDC (R5F)
MSC (multi-scalar) (R5F)
Pyramid (using MSC) (R5F)
Dense Optical Flow (R5F)
Stereo Disparity Engine (R5F)
BLNF (bilateral noise filter) (R5F)
CSI2-RX camera (R5F)
CSI2-TX (R5F)
Following are not yet functional in this release (due to pending driver dependencies):
Display (eDP and HDMI) (R5F)
Display M2M (R5F)
OpenVX tutorials for getting started
PyTIOVX tools for target kernel code generation
Performance Analyzer tool for run time logging of OpenVX graphs
5.11.1.2.6. Imaging¶
Note
None of the items listed in this section are tested yet due to pending Display dependencies of tests.
IMX390 2MP sensor driver (30/60fps) with IQ tuning
AR0233 2.5MP sensor driver with IQ tuning
AR0820 8MP sensor driver with IQ tuning
TI Auto-exposure and auto white-balance algorithms
Support for UB960 broadcast mode
Live Tuning Runtime interaction with PC tuning tool over Ethernet
Sensor framework supports heterogeneous camera support
5.11.1.2.7. TI Autonomous Driving Algorithms (TIADALG)¶
Image pre-processing APIs for color plane conversion and separation YUV to RGB for DL applications (C6x optimized. recompiled for C7x)
5.11.1.2.8. FreeRTOS¶
FreeRTOS for R5F and C7x
5.11.1.2.9. Code Gen Tools (CGT)¶
TI Compiler, assembler, linker for R5F, C7x
LLVM/TI CLANG (1.3 LTS) for R5F.
GCC compiler for A72 (needs to be downloaded separately)
5.11.2. Device Support and Validation Information¶
SoC |
Build Host (OS) |
Run Target (OS) |
Test Plaform |
---|---|---|---|
J721S2 |
x86_64 (Linux Ubuntu 18.04) |
R5F, C7x running FreeRTOS A72 running Linux |
J721S2 EVM with daughter cards |
PC emulation mode (1) |
x86_64 (Linux Ubuntu 18.04) |
x86_64 (Linux Ubuntu 18.04) |
x86_64 (Linux Ubuntu 18.04) |
(1) Requires download of addon package from mySecure Software
5.11.3. Upgrade and Compatibility¶
In this section, we only highlight a few significant changes in this SDK. For full list of upgrade and compatibility topics, please refer to individual components release notes SDK Components.
5.11.4. Known Issues¶
Record ID |
Summary |
Workaround |
Impact |
---|---|---|---|
Clock tree review still in progress for DM to ensure all clocks are present in the device |
|||
ADASVISION-5063 |
Main R5FSS is booting in secure mode which makes disables the cache coherency between the A72 (insecure) and R5F (secure) on the DDR shared memory region |
Cache on the A72 for this shared memory region is disabled |
Reduced performance will be seen when A72 reads or writes from/to the shared region (such as with reading outputs from the graph to store on an SD card) |
ADASVISION-5064 |
OCMC RAM init failure on MCU2-0 |
Init is disabled and memory previously mapped here is instead mapped to DDR |
Reduced performance of memory previously accessed from this region. In SDK this was only used by heterogeneous camera context save/restore |
ADASVISION-5065 |
The MCU2-1 and C7X-2 often fail to boot on a cold boot |
After a power-on boot invoke a warm “reboot” |
Extra linux boot upon power on. |
ADASVISION-5067 |
C7X-2 MMU table gets corrupted during initialization |
Added 10s delay during init of firmware |
Extra delay during boot. |
Refer to individual SDK Components release notes for known issues in each component
5.11.5. Additional Reports¶
Test reports, traceability matrix not available yet for EA Release.