9.2. Understanding bootloaders in Processor SDK J721S2 (RTOS/Linux)¶
9.2.1. Introduction¶
There are two bootloaders in Processor SDK J721S2 (RTOS/Linux). They are:
RTOS Bootloader
Linux Bootloader
This developer note describes about these two bootloaders.
9.2.2. RTOS Bootloader¶
RTOS Bootloader is referred to as SBL (Secondary bootloader).
This is included in Processor SDK RTOS at
pdk_<device>_<version>/packages/ti/boot
This is used when all cores on the SoC run FreeRTOS
In this case one would see below boot files in a SD card
tiboot3.bin - this is the SBL which the ROM bootloader will boot on MCU R5F Core0
tiboot3.bin will boot tifs.bin - this is the DMSC firmware binary
tiboot3.bin will boot a file called “app” - this file contains binaries of all other CPUs like A72, Main R5F, C7x
“app” is created by running an offline tool which covert elf .out files to .rprc format and then combines these to something called “multi-core image”
See also
See this page for more info on this .rprc file and offline boot tools LINK
The table below provides more information about the features and differences between the SBL bootloader and the MCUSW “CAN Boot App”:
Feature area |
SBL Description |
MCUSW “CAN Boot App” |
Key Diffs / Comments |
---|---|---|---|
Initial Bootloader |
YES |
NO |
MCUSW CAN Boot app is a “tertiary” bootloader |
SoC’s Supported |
AM65xx/J7200/J721E/J721S2/J784S4 |
J7200/J721E/J721S2/J784S4 |
|
Device types supported |
GP, HS |
GP, HS |
NOTE: most, but not all, features are supported for each device type. Check specific feature support listed in each release. |
Runs on MCU R5F |
YES |
YES |
NOTE: the SBL is used to boot the MCUSW CAN Boot App |
Can support startup with MCU domain only |
YES |
YES |
|
Boot media supported |
UART, MMCSD, OSPI |
MMCSD, OSPI |
UART boot supported with SBL only |
Supports booting HLOS + RTOS images |
YES |
YES |
SBL uses “combined appimage” build to put all RTOS & HLOS images into a single .appimage, whereas a specific format of combined images is used with the CAN boot app. |
Boots another app to MCU R5F |
YES |
Boot app doesn’t support booting an app to the MCU R5F (since it is the app already running on that processor) |
|
Early CAN response demo |
NO |
YES |
|
Image Layout |
single appimage |
3-5 different appimages |
SBL: all images for the remote cores to be booted must all be combined in to a single .appimage file that is either placed on the SD card (for MMCSD boot) or is flashed to a single flash addr location (for xSPI / OSPI boot). This includes all HLOS & RTOS images that must be booted. MCUSW “CAN Boot App”: images for remote cores to be booted are split up into 3-5 different appimage files for either SD card booting or flashed into 3-5 different flash addresses for xSPI / OSPI booting (see details in the MCUSW CAN Boot App documentation). |
Doc links |
9.2.3. Linux Bootloader¶
Linux bootloader uses SPL and uboot to boot various CPUs.
This is included in Processor SDK Linux at below path
board-support/u-boot-<version and git tag>
This is used when Linux runs on A72. Most SDK demos like deep learning demos use Linux on A72 hence this bootloader is used in many out of box demos.
In this case one would see below files in the SD card
tiboot3.bin - this is the SPL (not SBL) which the ROM bootloader will boot on MCU R5F Core0
tiboot3.bin will boot tifs.bin - this is the SMS firmware binary
tiboot3.bin will boot tispl.bin on A72 - this is the 1st stage bootloader on A72 before uboot
tispl.bin on A72 will boot uboot.img on A72 - this is uboot which will boot Linux
uboot.img will boot non A72 (such as C7x, R5F) binaries located at below path in rootfs partition of the SD card
/lib/firmware/j721s2-<cpu>-fw
uboot.img will read a file uEnv.txt which will tell which .dtbo files to apply in addition to below dtb file present in rootfs partition
/boot/k3-j721s2-proc-board-tps65917.dtb
uboot.img will boot Linux kernel stored in rootfs partition below
/boot/Image
Linux will use information in the loaded .dtb/dtbo files to configure itself during boot
Note
Steps 4-8 is standard Linux boot flow typical of any SoC.
Steps 1-3 are specific to J7 SoC.
See also
Refer to PSDK LINUX documentation for more information on uboot https://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-j721s2/latest/exports/docs/linux/Foundational_Components_U-Boot.html#u-boot-user-s-guide
9.2.4. Bootloaders Supported in Vision Apps¶
Vision Apps supports both Linux and QNX running on the A72. (For more information, see LINK).
Along with the support for each of these HLOS’s, Vision Apps provides a set of scripts which allow developers to quickly build and run with different bootloaders. A summary of these bootloader support for each of these builds can be seen in the table below:
HLOS |
U-boot SPL |
SBL MCUSW “CAN Boot App” |
DM |
---|---|---|---|
Linux |
YES (Default) |
NO |
Default DM with U-boot SPL is from PDK, but vision apps binary can be built using vision apps build flags |
QNX |
YES |
YES (Default) |
Default DM with U-boot SPL is from PDK, but vision apps binary can be built using vision apps build flags. For SBL MCUSW “CAN Boot App”, the boot app serves as the DM. |
9.2.5. Bootloader Memory Map¶
Details about various bootloader components’ memory maps are provided below. This may be needed in the case that a custom bootloader needs to be created.
Component |
Memory Map Location Link |
---|---|
R5 SPL |
|
SYSFW |
|
DMSC ROM |
Please reference the Initialization Chapter of the Boot Memory Maps section of the TRM |