2.8. Release Notes - 08_00_03¶
2.8.1. Introduction¶
2.8.2. What’s New¶
- This is the early adopter release for J721S2.This package contains drivers required for J721S2 platform only.
PDK modules validated on J721S2 EVM:
Module |
A72 |
R5F |
C7x |
---|---|---|---|
FreeRTOS/OSAL |
NA |
YES |
YES |
SCICLIENT |
YES |
YES |
YES |
UART |
YES |
YES |
YES |
UDMA |
YES |
YES |
YES |
IPC |
YES |
YES |
YES |
OSPI |
NO |
YES |
NA |
MCSPI |
NA |
YES |
NA |
MMCSD |
YES |
YES |
NA |
VHWA |
NA |
YES |
NA |
CSIRX |
NA |
YES |
NA |
CSITX |
NA |
YES |
NA |
GPIO |
YES |
YES |
NA |
CRC(CSL) |
YES |
NA |
NA |
VTM(CSL) |
NA |
YES |
NA |
SPINLCOK(CSL) |
YES |
YES |
NA |
ESM(CSL) |
NA |
YES |
NA |
DMTIMER(CSL) |
NA |
YES |
NA |
DCC(CSL) |
NA |
YES |
NA |
UART(CSL) |
YES |
YES |
NA |
MCAN(CSL) |
NA |
YES |
NA |
VIM(CSL) |
NA |
YES |
NA |
ECC(CSL) |
NA |
YES |
NA |
- SBL Boot Modes:
UART, MMC, OSPI
Internal Memory, DDR
DMA mode, non-DMA mode
- Board Diagnostic
DDR
Board ID EEPROM
Boot EEPROM
UART
SD card
eMMC
OSPI NOR Flash
QSPI Flash
Current Monitor
Temperature sensor
On board RTC
User LED
Automation Header
- Uniflash
OSPI NOR Flash
OSPI NAND Flash
2.8.3. Device Support¶
J721S2 EVM (BOARD=j721s2_evm)
2.8.4. CCS Setup¶
Refer :CCS Setup for J721S2
2.8.5. Validation Information¶
2.8.6. Tool Chain Information¶
Component |
Version |
---|---|
FreeRTOS Kernel |
10.4.3 |
lwIP stack |
2.1.2 |
lwIP-contrib |
2.1.0 |
XDC Tools |
3_61_04_40 |
TI ARM CLANG |
1.3.0.LTS |
TI C7x code generation tools |
2.0.1.STS |
GCC ARM code generation tools |
ARCH64 9.2-2019.12 |
2.8.7. Known Issues¶
Key |
Summary |
Module |
Reported in Release |
Affected Platforms |
Workaround in this release |
---|---|---|---|---|---|
DK-10850 |
Scicleint_rmRingCfg API is not programming BCDMA Ring Cfg Register |
SCICLIENT |
PROCESSOR-SDK_08.00.03 |
J7AEP |
WA added in UDMA Driver to program the same |
PDK-10849 |
Sciclient_rmIrqSet is not programming Interrupt Aggregator Unmapped Event Mapping Register for BCDMA events |
SCICLIENT |
PROCESSOR-SDK_08.00.03 |
J7AEP |
WA added in UDMA Driver to program the same |
PDK-10847 |
UART DMA UT is hanging on mcu1_0/mcu1_1 |
UART |
PROCESSOR-SDK_08.00.03 |
J7AEP |
Use Non-DMA mode |
PDK-10829 |
Sciclient UT in Interrupt mode is hanging on C7x cores |
SCICLIENT |
PROCESSOR-SDK_08.00.03 |
J7AEP |
Use polling mode |
PDK-10827 |
McSPI DMA UT is not functional |
SPI |
PROCESSOR-SDK_08.00.03 |
J7AEP |
Individual tests works fine |
2.8.8. Limitations¶
DSS is not yet up.
VISS-> MSC Flexconnect is not yet up.