5.5.8.1.5.1. Enet TSN GPTP Example¶
5.5.8.1.5.1.1. Makefile¶
For an example of the app makefile, please refer to <enet>/examples/enet_tsn/enet_tsn_gptp_example/makefile.
There are some important notes to consider:
To include TSN components, add the following macros:
INCLUDE_INTERNAL_INTERFACES += tsn_gptp tsn_combase tsn_unibase tsn_uniconf COMP_LIST_COMMON += tsn_combase tsn_unibase tsn_gptp tsn_uniconf mmcsd fatfs_indp
Ensure that the
tsninit.c,gptp_init.c``and ``debug_log.cfiles are included in the app’s source:SRCS_COMMON += main.c tsninit.c gptp_init.c debug_log.c
If the log task is used, define the
TSN_USE_LOG_BUFFERmacro:CFLAGS_LOCAL_COMMON += -DTSN_USE_LOG_BUFFER=1
5.5.8.1.5.1.2. Build Enet TSN GPTP example¶
Navigate to the <pdk>/packages/ti/build directory:
$ cd <pdk>/packages/ti/build
Build the TSN modules (tsn_unibase, tsn_combase, tsn_gptp, tsn_uniconf):
$ make tsn_unibase tsn_combase tsn_gptp tsn_uniconf
To clean the build and remove generated files:
$ make tsn_unibase_clean tsn_combase_clean tsn_gptp_clean tsn_uniconf_clean
You can specify the build mode as either release or debug. By default, the release mode is built. To build in debug mode, use the
BUILD_PROFILE=debugoption:$ make tsn_unibase tsn_combase tsn_gptp tsn_uniconf BUILD_PROFILE=debug
If you want to build with C++ compiling rules, use the
CPLUSPLUS_BUILD=yesoption:$ make tsn_unibase tsn_combase tsn_gptp tsn_uniconf CPLUSPLUS_BUILD=yes
To build the TSN GPTP example app in the PDK, use the following command:
$ make enet_tsn_gptp_example_freertos CORE=mcu2_0
The example app binary file can be found at the following location:
<pdk>/packages/ti/binary/enet_tsn_example_freertos/bin/j7200_evm/enet_tsn_gptp_example_freertos_mcu2_0_release.xer5f
This command will build the TSN example app (
enet_tsn_gptp_example_freertos) using the FreeRTOS operating system and targeting the mcu2_0 core. Adjust the command according to your specific requirements, such as selecting a different operating system or core if needed.
5.5.8.1.5.1.3. Running Enet TSN GPTP example¶
Launch a CCS debug session, load and run
enet_tsn_gptp_example_freertos_mcu2_0_release.xer5fbinary file to the MAIN_Cortex_R5_0_0. Alternatively, the example application can be loaded using any other boot method such as MMC/SD.Logs will be printed in Main UART port 0. Below is an example of the log when gPTP works in slave mode:
========================== TSN Example App ========================== EnetBoard_setupPorts: 2 of 2 ports configurations found Configuring SerDes lane 2 for QSGMII EnetApp_appInitTask: EnetBoard_setupPorts() done EnetApp_appInitTask: EnetApp_init() done Start: uniconf_task EnetApp_uniconfTask: dbname: NULL EnetMcm: CPSW_5G on MAIN NAVSS Mdio_open: MDIO manual mode enabled PHY 16 is alive PHY 17 is alive PHY 18 is alive PHY 19 is alive EnetPhy_bindDriver: PHY 16: OUI:0001c1 Model:27 Ver:00 <-> 'vsc8514' : OK EnetPhy_bindDriver: PHY 17: OUI:0001c1 Model:27 Ver:00 <-> 'vsc8514' : OK Logger_task: started unibase-1.1.5-jacinto INF:cbase:tilld0: has mac: 00:00:00:00:00:00 INF:cbase:tilld1: has mac: 00:00:00:00:00:00 INF:cbase:cb_lld_task_create: uniconf_task stack_size=16384 INF:uconf:simpledb_open:no data is imported INF:uconf:get_next_nameid:a new mod=xl4-data, enum=0 INF:uconf:get_next_nameid:a new mod=xl4-extmod, enum=1 INF:uconf:uc_hwal_open: INF:cbase:cb_rawsock_open:combase-1.1.4-jacinto INF:cbase:cb_rawsock_open:dmaTxChId=-1 numRxChannels=0 dmaRxChId=-1 nTxPkts=0 nRxPkts=0 pktSize=0 INF:cbase:tilld0: alloc mac: 70:FF:76:1D:A5:C8 INF:uconf:get_next_nameid:a new mod=ietf-interfaces, enum=2 INF:uconf:get_next_nameid:a new mod=ieee1588-ptp-tt, enum=3 INF:uconf:get_next_nameid:a new mod=ieee802-dot1q-bridge, enum=4 INF:uconf:get_next_nameid:a new mod=ieee802-dot1ab-lldp, enum=5 INF:uconf:get_next_nameid:a new mod=ieee802-dot1q-tsn-config-uni, enum=6 INF:uconf:get_next_nameid:a new mod=excelfore-tsn-remote, enum=7 INF:uconf:get_next_nameid:a new mod=excelfore-netconf-server, enum=8 INF:uconf:get_next_nameid:a new mod=ietf-netconf-monitoring, enum=9 INF:uconf:get_next_nameid:a new mod=ietf-yang-library, enum=10 INF:uconf:create_semname_with_dbname:null dbname is specified. INF:cbase:cb_lld_task_create: uniconf_hwal_thread stack_size=16384 INF:uconf:000000-569508:uniconf_main:uniconf started EnetApp_gptpYangConfig:domain=0 EnetApp_gptpYangConfig:domain=1 EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_SINGLE_CLOCK_MODE=1 EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_USE_HW_PHASE_ADJUSTMENT=1 EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_CLOCK_COMPUTE_INTERVAL_MSEC=100 EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_FREQ_OFFSET_IIR_ALPHA_START_VALUE=1 EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_FREQ_OFFSET_IIR_ALPHA_STABLE_VALUE=4 EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_PHASE_OFFSET_IIR_ALPHA_START_VALUE=1 EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_PHASE_OFFSET_IIR_ALPHA_STABLE_VALUE=4 EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_MAX_DOMAIN_NUMBER=2 EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_CMLDS_MODE=1 EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_SECOND_DOMAIN_THIS_CLOCK=1 Start: gptp2d_task Start: estapp_task EnetApp_initTsn:gptp start done! CPU Load: 65% INF:cbase:cbl_query_response:tilld0 link DOWN !!!! INF:cbase:cbl_query_response:tilld1 link DOWN !!!! INF:cbase:tilld1: alloc mac: 70:FF:76:1D:A5:C9 INF:uconf:get_next_nameid:a new extmod=xl4gptp, enum=0 INF:uconf:create_semname_with_dbname:null dbname is specified. INF:cbase:cb_lld_task_create: gptp2d_task stack_size=16384 INF:cbase:cb_lld_task_create: estapp_task stack_size=16384 INF:cbase:cb_rawsock_open:combase-1.1.4-jacinto INF:cbase:cb_rawsock_open:dmaTxChId=1 numRxChannels=0 dmaRxChId=-1 nTxPkts=0 nRxPkts=0 pktSize=0 INF:gptp:gptpman_run:max_domains=2, max_ports=2 INF:cbase:cb_rawsock_open:combase-1.1.4-jacinto INF:cbase:cb_rawsock_open:dmaTxChId=8 numRxChannels=0 dmaRxChId=-1 nTxPkts=0 nRxPkts=0 pktSize=0 INF:cbase:DmaOpen: TxChNum 1 INF:cbase:DmaOpen: Rx startIdx 84 flowId 1 INF:gptp:gptpmasterclock_init: gptp2-1.2.4-jacinto, ref_counter=1 INF:gptp:gptpmasterclock_init:failed INF:gptp:gptpmasterclock_close: ref_counter=0 INF:cbase:DmaOpen: TxChNum 8 INF:gptp:gptpmasterclock_init: gptp2-1.2.4-jacinto, ref_counter=0 INF:gptp:gptpmasterclock_close: ref_counter=-1 INF:cbase:DmaOpen: Rx startIdx 84 flowId 2 INF:cbase:LLDEnetFilter:destmac:01:80:C2:00:00:0E, vlanId:0, ethType:0x88f7 INF:gptp:dev:tilld0 open success INF:gptp:dev:tilld1 open success INF:gptp:gptpnet_init:Open lldtsync OK! INF:gptp:IEEE1588-2019 performance monitoring disabled. INF:gptp:IEEE1588-2019 performance monitoring disabled. INF:gptp:gptpclock_mode_slave_main:domainIndex=0 already in SLAVE_MAIN INF:uconf:ydbi_get_item_ifk3vk0:no data INF:uconf:ydbi_get_item_ifk3vk0:no data INF:gptp:onenet_activate:tilld0 status=0, duplex=1, speed=0Mbps INF:uconf:ydbi_get_item_ifk3vk0:no data INF:uconf:ydbi_get_item_ifk3vk0:no data INF:gptp:onenet_activate:tilld1 status=0, duplex=1, speed=0Mbps INF:ubase:GPTP_MEDIUM_ALLOC: fragsize=16 fragused/fragnum=1301/2271 (57%) INF:ubase:GPTP_SMALL_ALLOC: fragsize=4 fragused/fragnum=34/126 (26%) INF:ubase:SM_DATA_INST: fragsize=8 fragused/fragnum=3770/7222 (52%) INF:gptp:gptpman_run:GPTPNET_INTERVAL_TIMEOUT_NSEC=125000000 INF:gptp:gptpmasterclock_init: gptp2-1.2.4-jacinto, ref_counter=0 INF:gptp:000001-377231:domainIndex=0, GM changed old=00:00:00:00:00:00:00:00, new=70:FF:76:FF:FE:1D:A5:C8 INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=2 INF:gptp:set_phase_offsetGM:domainIndex=0, New adjustment(New GM?) INF:gptp:000001-379710:domainIndex=1, GM changed old=00:00:00:00:00:00:00:00, new=70:FF:76:00:01:1D:A5:C8 INF:gptp:000001-379787:adjust_GM_btw_domains:domainIndex=1 INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=1, gmstate=2 INF:gptp:set_phase_offsetGM:domainIndex=1, New adjustment(New GM?) CpswMacPort_checkSgmiiStatus: MAC 1: SGMII link parter config port: link up: 1-Gbps Full-Duplex Cpsw_handleLinkUp: Port 1: Link up: 1-Gbps Full-Duplex MAC Port 1: link up INF:cbase:cbl_query_response:tilld0: link UP, speed=1000, duplex=1 !!!! INF:gptp:index=1 speed=1000, duplex=full INF:gptp:md_pdelay_resp_sm_recv_req:port=1, set receivedNonCMLDSPdelayReq=-1 WRN:gptp:000004-877107:waiting_for_pdelay_interval_timer_proc:portIndex=1, sourcePortIdentity=70:FF:76:FF:FE:1D:9B:42, thisClock=70:FF:76:FF:FE:1D:A5:C8, neighborPropDelay=659 INF:gptp:waiting_for_pdelay_interval_timer_proc:portIndex=1, not asCapable INF:gptp:set neighborGptpCapable, domainIndex=0, portIndex=1 INF:gptp:set neighborGptpCapable, domainIndex=1, portIndex=1 INF:gptp:set asCapable for domainIndex=0, portIndex=1 INF:gptp:000005-000614:gptpgcfg_set_asCapable:domainInde=0, portIndex=1, ascapable=1 INF:gptp:000005-000978:gm_stable:gm_unstable_proc:domainIndex=0 INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=1 INF:gptp:000005-001099:active domain switched from 0 to 1 INF:gptp:000005-001154:gm_stable:gm_unstable_proc:domainIndex=0 INF:gptp:set asCapable for domainIndex=1, portIndex=1 INF:gptp:000005-001610:gptpgcfg_set_asCapable:domainInde=1, portIndex=1, ascapable=1 INF:gptp:000005-001922:gm_stable:gm_unstable_proc:domainIndex=1 INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=1, gmstate=1 INF:gptp:000005-002079:gm_stable:gm_unstable_proc:domainIndex=1 INF:gptp:000005-125310:setSyncTwoStep_txSync:domainIndex=0, portIndex=1, sync gap=5125msec INF:gptp:000005-125665:setSyncTwoStep_txSync:domainIndex=1, portIndex=1, sync gap=5125msec INF:gptp:000005-125954:setFollowUp_txFollowUp:domainIndex=0, portIndex=1, fup gap=5125msec INF:gptp:000005-126689:setFollowUp_txFollowUp:domainIndex=1, portIndex=1, fup gap=5125msec INF:gptp:000005-812183:domainIndex=0, GM changed old=70:FF:76:FF:FE:1D:A5:C8, new=70:FF:76:FF:FE:1D:9B:42 INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=0 INF:gptp:000005-812374:gm_stable:gm_unstable_proc:domainIndex=0 INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=1 INF:gptp:000005-813160:domainIndex=1, GM changed old=70:FF:76:00:01:1D:A5:C8, new=70:FF:76:00:01:1D:9B:42 INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=1, gmstate=0 INF:gptp:000005-813377:gm_stable:gm_unstable_proc:domainIndex=1 INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=1, gmstate=1 INF:gptp:set_phase_offsetGM:domainIndex=0, New adjustment(New GM?) INF:gptp:set_phase_offsetGM:domainIndex=0, offset adjustment, diff=885934511 INF:gptp:set_phase_offsetGM:domainIndex=1, New adjustment(New GM?) INF:gptp:set_phase_offsetGM:domainIndex=1, offset adjustment, diff=885926319 WRN:gptp:000005-876210:waiting_for_pdelay_interval_timer_proc:portIndex=1, sourcePortIdentity=70:FF:76:FF:FE:1D:9B:42, thisClock=70:FF:76:FF:FE:1D:A5:C8, neighborPropDelay=663 INF:gptp:waiting_for_pdelay_interval_timer_proc:portIndex=1, not asCapable INF:gptp:set_phase_offsetGM:domainIndex=0, offset adjustment by Freq., diff=10726 INF:gptp:set_phase_offsetGM:domainIndex=1, New adjustment(New GM?) INF:gptp:set_phase_offsetGM:domainIndex=1, offset adjustment, diff=-885923142 INF:gptp:set_phase_offsetGM:domainIndex=0, stable INF:gptp:clock_master_sync_receive:computeGmRateRatio:domainIndex=0 unstable rate=-6989ppb (timeleap_past) IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 2863ppb, GMdiff=9852nsec INF:gptp:set_phase_offsetGM:domainIndex=1, stable IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -3252ppb, GMdiff=8812nsec INF:gptp:clock_master_sync_receive:computeGmRateRatio:domainIndex=1 unstable rate=-27314ppb (timeleap_past) IFV:gptp:domainIndex=1, clock_master_sync_receive:the master clock rate to -28164ppb, GMdiff=-3397nsec IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -6603ppb, GMdiff=8139nsec IFV:gptp:domainIndex=1, clock_master_sync_receive:the master clock rate to 127041ppb, GMdiff=15511nsec IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -8396ppb, GMdiff=7675nsec IFV:gptp:domainIndex=1, clock_master_sync_receive:the master clock rate to 131519ppb, GMdiff=15584nsec IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -9324ppb, GMdiff=7330nsec IFV:gptp:domainIndex=1, clock_master_sync_receive:the master clock rate to 123236ppb, GMdiff=14108nsec IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -9876ppb, GMdiff=7041nsec IFV:gptp:domainIndex=1, clock_master_sync_receive:the master clock rate to 145557ppb, GMdiff=16386nsec IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -10168ppb, GMdiff=6791nsec IFV:gptp:domainIndex=1, clock_master_sync_receive:the master clock rate to 126690ppb, GMdiff=13579nsec INF:gptp:000006-875368:gm_stable:gm_stable_proc:domainIndex=0 INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=2 INF:gptp:000006-875495:active domain switched from 1 to 0 INF:gptp:000006-875657:gm_stable:gm_stable_proc:domainIndex=1 INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=1, gmstate=2 INF:gptp:waiting_for_pdelay_interval_timer_proc:set asCapableAcrossDomains, portIndex=1 IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -10494ppb, GMdiff=6547nsec IFV:gptp:domainIndex=1, clock_master_sync_receive:the master clock rate to 160372ppb, GMdiff=17219nsec IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -10622ppb, GMdiff=6333nsec IFV:gptp:domainIndex=1, clock_master_sync_receive:the master clock rate to 141435ppb, GMdiff=14401nsec IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -10747ppb, GMdiff=6126nsec IFV:gptp:domainIndex=1, clock_master_sync_receive:the master clock rate to 107379ppb, GMdiff=9837nsec IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -10915ppb, GMdiff=5920nsec IFV:gptp:domainIndex=1, clock_master_sync_receive:the master clock rate to 122709ppb, GMdiff=11397nsec IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -10936ppb, GMdiff=5738nsec IFV:gptp:domainIndex=1, clock_master_sync_receive:the master clock rate to 150238ppb, GMdiff=14389nsec IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -16343ppb, GMdiff=-402nsec IFV:gptp:domainIndex=1, clock_master_sync_receive:the master clock rate to 132452ppb, GMdiff=-1743nsec IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -16415ppb, GMdiff=-389nsec IFV:gptp:domainIndex=1, clock_master_sync_receive:the master clock rate to 137973ppb, GMdiff=-1021nsec IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -16462ppb, GMdiff=-367nsec IFV:gptp:domainIndex=1, clock_master_sync_receive:the master clock rate to 126943ppb, GMdiff=-2327nsec IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -16514ppb, GMdiff=-349nsec IFV:gptp:domainIndex=1, clock_master_sync_receive:the master clock rate to 143256ppb, GMdiff=-279nsec IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -16560ppb, GMdiff=-331nsec IFV:gptp:domainIndex=1, clock_master_sync_receive:the master clock rate to 129506ppb, GMdiff=-1937nsec IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -16583ppb, GMdiff=-304nsec ...
5.5.8.1.5.1.4. Verification¶
Single port
Connect a port to a Linux PC and run gptp2d from the PC.
The expected log from the slave side will be stable and reprinted like this:
INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 65499ppb
INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 61563ppb
INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 58249ppb
INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 55383ppb
...
Instead of displaying the clock_master_sync_receive:... log, the following log
will be printed in the case of the master log:
domain=0, offset=0nsec, hw-adjrate=0ppb
gmsync=true, last_setts64=0nsec
domain=0, offset=0nsec, hw-adjrate=0ppb
gmsync=true, last_setts64=0nsec
CPU Load: 2%
domain=0, offset=0nsec, hw-adjrate=0ppb
gmsync=true, last_setts64=0nsec
CPU Load: 2%
domain=0, offset=0nsec, hw-adjrate=0ppb
gmsync=true, last_setts64=0nsec
CPU Load: 2%
domain=0, offset=0nsec, hw-adjrate=0ppb
gmsync=true, last_setts64=0nsec
...
Multiple ports
In this function, gPTP is operating as a switch. The availability of this feature is determined by the board configuration rather than the gPTP stack. If a board enables multiple MAC ports, the gPTP function should operate properly. To test this function, please connect two PCs to two ports of the EVM.
When the EVM board acts as the master, only the master log will be printed out, while the two PCs will print the slave log. On the other hand, if one of the PCs acts as the master, the slave log will be printed by the other PC and the EVM, while the master PC will print the master log.
To identify which machine is the master, please check the log:
INF:gptp:001809-750000:domainIndex=0, GM changed old=24:76:25:FF:FE:96:6C:41, new=70:FF:76:FF:FE:1D:9B:77
In this case, the machine with the source MAC address of 70:FF:76:FF:FE:1D:9B:77 is the master.