Kernel for computing vector division floating point values.
- The kernel support computation of division of a batch of several inputs in one kernel call.
- The buffer used for providing input data may be required to be bigger than data size itself. The actual size required to be allocated for the input buffer
|
| int32_t | MATHLIB_div_getHandleSize (MATHLIB_div_InitArgs *pKerInitArgs) |
| | This is a query function to calculate the size of internal handle. More...
|
| |
| MATHLIB_STATUS | MATHLIB_div_init (MATHLIB_kernelHandle handle, MATHLIB_bufParams1D_t *bufParamsIn, MATHLIB_bufParams1D_t *bufParamsOut, const MATHLIB_div_InitArgs *pKerInitArgs) |
| | This function should be called before the MATHLIB_div_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle. More...
|
| |
| MATHLIB_STATUS | MATHLIB_div_init_checkParams (MATHLIB_kernelHandle handle, const MATHLIB_bufParams2D_t *bufParamsIn, const MATHLIB_bufParams2D_t *bufParamsOut, const MATHLIB_div_InitArgs *pKerInitArgs) |
| | This function checks the validity of the parameters passed to MATHLIB_div_init function. This function is called with the same parameters as the MATHLIB_div_init, and this function must be called before the MATHLIB_div_init is called. More...
|
| |
| MATHLIB_STATUS | MATHLIB_div_exec (MATHLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| | This function is the main kernel compute function. More...
|
| |
| MATHLIB_STATUS | MATHLIB_div_exec_checkParams (MATHLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut) |
| | This function checks the validity of the parameters passed to MATHLIB_div_exec function. This function is called with the same parameters as the MATHLIB_div_exec, and this function must be called before the MATHLIB_div_exec is called. More...
|
| |
| void | MATHLIB_div_perfEst (MATHLIB_kernelHandle handle, const MATHLIB_bufParams2D_t *bufParamsIn, const MATHLIB_bufParams1D_t *bufParamsFilterCoeff, const MATHLIB_bufParams2D_t *bufParamsFilterVar, const MATHLIB_bufParams2D_t *bufParamsOut, uint64_t *archCycles, uint64_t *estCycles) |
| | This is a utility function that gives an estimate of the cycles consumed for the kernel execution. More...
|
| |
◆ MATHLIB_div_getHandleSize()
This is a query function to calculate the size of internal handle.
- Parameters
-
| [in] | pKerInitArgs | : Pointer to structure holding init parameters |
- Returns
- Size of the buffer in bytes
◆ MATHLIB_div_init()
This function should be called before the MATHLIB_div_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [in] | bufParamsFilter | : Pointer to the structure containing dimensional information of filter buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
- Returns
- Status value indicating success or failure. Refer to MATHLIB_STATUS.
◆ MATHLIB_div_init_checkParams()
This function checks the validity of the parameters passed to MATHLIB_div_init function. This function is called with the same parameters as the MATHLIB_div_init, and this function must be called before the MATHLIB_div_init is called.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of output buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
- Returns
- Status value indicating success or failure. Refer to MATHLIB_STATUS.
◆ MATHLIB_div_exec()
This function is the main kernel compute function.
Please refer to details under MATHLIB_div_exec
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [out] | pOut | : Pointer to buffer holding the output data |
- Returns
- Status value indicating success or failure. Refer to MATHLIB_STATUS.
- Assumptions:
-
- Performance Considerations:
- For best performance,
- the input and output data buffers are expected to be in L2 memory
- the buffer pointers are assumed to be 64-byte aligned
◆ MATHLIB_div_exec_checkParams()
This function checks the validity of the parameters passed to MATHLIB_div_exec function. This function is called with the same parameters as the MATHLIB_div_exec, and this function must be called before the MATHLIB_div_exec is called.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [in] | pFilter | : Pointer to buffer holding the input data |
| [out] | pOut | : Pointer to buffer holding the output matrix |
- Returns
- Status value indicating success or failure. Refer to MATHLIB_STATUS.
◆ MATHLIB_div_perfEst()
This is a utility function that gives an estimate of the cycles consumed for the kernel execution.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of the input buffer |
| [in] | bufParamsFilter | : Pointer to the structure containing dimensional information of the filter buffer |
| [in] | bufParamsOut | : Pointer to the structure containing dimensional information of the output buffer |
| [out] | archCycles | : Cycles estimated for the compute, startup and teardown |
| [out] | estCycles | : Cycles estimated for the compute, startup, teardown and any associated overhead |