![]() |
PDK API Guide for J721S2
|
Interface file for MSC M2M FVID2 driver
Files | |
| file | vhwa_m2mMsc.h |
| Defines the structures / control operations that could be used to configure / control MSC M2M driver. | |
Data Structures | |
| struct | Vhwa_M2mMscSecChPrms |
| Connfiguration parameters MSC secondary channel. [ Only applicable for VPAC3. NA for VPAC(J721E) ]. More... | |
| struct | Vhwa_M2mMscParams |
| Connfiguration parameters of MSC. More... | |
| struct | Vhwa_M2mMscCreatePrms |
| Parameters required to create a new handle. More... | |
| struct | Vhwa_M2mMscSl2AllocPrms |
| Init Parameters required to allocate MSC drivere. More... | |
| struct | Vhwa_M2mMscInitParams |
| Init Parameters for MSC M2M Driver. More... | |
| struct | Vhwa_M2mMscPerf |
| Structure for storing the performance numbers. More... | |
| struct | Vhwa_M2mMscPsaSign |
| Structure for storing PSA signatures. More... | |
Functions | |
| static void | Vhwa_m2mMscInitParamsInit (Vhwa_M2mMscInitParams *mscInitPrms) |
| Vhwa_M2mMscInitParams structure init function. More... | |
| static void | Vhwa_m2mMscParamsInit (Vhwa_M2mMscParams *mscCfg) |
| Function to initialize the MSC configuration parameters to default. More... | |
| static void | Vhwa_M2mMscCreatePrmsInit (Vhwa_M2mMscCreatePrms *createArgs) |
| Function to initialize the MSC create params to default. More... | |
| int32_t | Vhwa_m2mMscInit (const Vhwa_M2mMscInitParams *initPrms) |
| MSC initialization function. This function initializes the MSC hardware and drivers. This function should be called before calling any driver APIs and only once. More... | |
| int32_t | Vhwa_m2mMscDeInit (void) |
| MSC de-initialization function. This function un-initializes the MSC hardware and drivers. This function should be called during system shutdown if Vhwa_m2mMscDeInit() was called by the application. More... | |
| int32_t | Vhwa_m2mMscAllocSl2 (const Vhwa_M2mMscSl2AllocPrms *sl2allocPrms) |
| Function to allocate Sl2 memory for input and output buffers. More... | |
| int32_t | Vhwa_m2mMscFreeSl2 (void) |
| Function to free allocated SL2. More... | |
| static void | Vhwa_M2mMscSl2AllocPrmsInit (Vhwa_M2mMscSl2AllocPrms *sl2Prms) |
Macros | |
| #define | VPAC_MSC_INST_ID_0 (VHWA_M2M_VPAC_0_MSC_DRV_INST_ID_0) |
| Default MSC Instance/Thread ID 0 [For backward compatibility]. More... | |
| #define | VPAC_MSC_INST_ID_1 (VHWA_M2M_VPAC_0_MSC_DRV_INST_ID_1) |
| Default MSC Instance/Thread ID 1 [For backward compatibility]. More... | |
| #define | VHWA_M2M_MSC_MAX_INST (VHWA_M2M_VPAC_0_MSC_DRV_INST_ID_1 + 1U) |
| Maximum supported instance for MSC [For backward compatibility]. More... | |
| #define | VHWA_M2M_MSC_MIN_RD_BUFFER_DEPTH (6U) |
| Minimum supported depth value for read buffer in VHWA memory. More... | |
| #define | VHWA_M2M_MSC_MIN_WR_BUFFER_DEPTH (2U) |
| Minimum supported depth value for write buffer in VHWA memory. More... | |
| #define | VHWA_M2M_MSC_MAX_COMP (2u) |
| Maximum possible MSC iteration for a simgle request (Luma + Chroma) More... | |
| #define | VHWA_M2M_MSC_MAX_IN_CHANNEL (1u) |
| #define | VHWA_M2M_MSC_MAX_HANDLES (16u) |
| Max Number of handles supported for each instance of MSC M2M Driver. More... | |
VHWA MSC Instance ID | |
|
VHWA VPAC MSC Instance ID's. There are two parallel threads of MSC supported in HW for each VPAC instance | |
| #define | VHWA_M2M_VPAC_0_MSC_DRV_INST_ID_0 (0U) |
| VPAC 0 MSC Instance 0. More... | |
| #define | VHWA_M2M_VPAC_0_MSC_DRV_INST_ID_1 (1U) |
| VPAC 0 MSC Instance 1. More... | |
| #define | VHWA_M2M_MSC_DRV_NUM_INST (VHWA_M2M_VPAC_0_MSC_DRV_INST_ID_1 + 1U) |
| Total number of MSC instances. More... | |
MSC IOCTL macros | |
| #define | VHWA_M2M_IOCTL_MSC_SET_COEFF (VHWA_IOCTL_MSC_IOCTL_BASE) |
| IOCTL for Setting filter coefficients. More... | |
| #define | VHWA_M2M_IOCTL_MSC_SET_PARAMS (VHWA_M2M_IOCTL_MSC_SET_COEFF + 1U) |
| IOCTL for Setting MSC configuration. More... | |
| #define | VHWA_M2M_IOCTL_MSC_SET_BW_LIMITER (VHWA_M2M_IOCTL_MSC_SET_PARAMS + 1U) |
| IOCTL to set bandwidth limiter. This IOCTL take pointer to structure Vhwa_HtsLimiter as input. More... | |
| #define | VHWA_M2M_IOCTL_MSC_GET_PERF (VHWA_M2M_IOCTL_MSC_SET_BW_LIMITER + 1U) |
| IOCTL to get the IP performance. More... | |
| #define | VHWA_M2M_IOCTL_MSC_GET_PSA_SIGN (VHWA_M2M_IOCTL_MSC_GET_PERF + 1U) |
| IOCTL to get PSA signature for all enabeld outputs. More... | |
| #define | VHWA_M2M_IOCTL_MSC_REGISTER_ERR_CB (VHWA_M2M_IOCTL_MSC_GET_PSA_SIGN + 1U) |
| IOCTL for enabling error events and registering callbacks for the same. More... | |
| #define | VHWA_M2M_IOCTL_MSC_SYNC_START (VHWA_M2M_IOCTL_MSC_REGISTER_ERR_CB + 1U) |
| IOCTL to sync start each module This IOCTL doesn't configure any register and only enable pipeline to start processing. More... | |
| #define VHWA_M2M_VPAC_0_MSC_DRV_INST_ID_0 (0U) |
VPAC 0 MSC Instance 0.
| #define VHWA_M2M_VPAC_0_MSC_DRV_INST_ID_1 (1U) |
VPAC 0 MSC Instance 1.
| #define VHWA_M2M_MSC_DRV_NUM_INST (VHWA_M2M_VPAC_0_MSC_DRV_INST_ID_1 + 1U) |
Total number of MSC instances.
| #define VPAC_MSC_INST_ID_0 (VHWA_M2M_VPAC_0_MSC_DRV_INST_ID_0) |
Default MSC Instance/Thread ID 0 [For backward compatibility].
| #define VPAC_MSC_INST_ID_1 (VHWA_M2M_VPAC_0_MSC_DRV_INST_ID_1) |
Default MSC Instance/Thread ID 1 [For backward compatibility].
| #define VHWA_M2M_MSC_MAX_INST (VHWA_M2M_VPAC_0_MSC_DRV_INST_ID_1 + 1U) |
Maximum supported instance for MSC [For backward compatibility].
| #define VHWA_M2M_MSC_MIN_RD_BUFFER_DEPTH (6U) |
Minimum supported depth value for read buffer in VHWA memory.
| #define VHWA_M2M_MSC_MIN_WR_BUFFER_DEPTH (2U) |
Minimum supported depth value for write buffer in VHWA memory.
| #define VHWA_M2M_MSC_MAX_COMP (2u) |
Maximum possible MSC iteration for a simgle request (Luma + Chroma)
| #define VHWA_M2M_MSC_MAX_IN_CHANNEL (1u) |
| #define VHWA_M2M_MSC_MAX_HANDLES (16u) |
Max Number of handles supported for each instance of MSC M2M Driver.
| #define VHWA_M2M_IOCTL_MSC_SET_COEFF (VHWA_IOCTL_MSC_IOCTL_BASE) |
IOCTL for Setting filter coefficients.
| #define VHWA_M2M_IOCTL_MSC_SET_PARAMS (VHWA_M2M_IOCTL_MSC_SET_COEFF + 1U) |
IOCTL for Setting MSC configuration.
| #define VHWA_M2M_IOCTL_MSC_SET_BW_LIMITER (VHWA_M2M_IOCTL_MSC_SET_PARAMS + 1U) |
IOCTL to set bandwidth limiter. This IOCTL take pointer to structure Vhwa_HtsLimiter as input.
| #define VHWA_M2M_IOCTL_MSC_GET_PERF (VHWA_M2M_IOCTL_MSC_SET_BW_LIMITER + 1U) |
IOCTL to get the IP performance.
| #define VHWA_M2M_IOCTL_MSC_GET_PSA_SIGN (VHWA_M2M_IOCTL_MSC_GET_PERF + 1U) |
IOCTL to get PSA signature for all enabeld outputs.
| #define VHWA_M2M_IOCTL_MSC_REGISTER_ERR_CB (VHWA_M2M_IOCTL_MSC_GET_PSA_SIGN + 1U) |
IOCTL for enabling error events and registering callbacks for the same.
| #define VHWA_M2M_IOCTL_MSC_SYNC_START (VHWA_M2M_IOCTL_MSC_REGISTER_ERR_CB + 1U) |
IOCTL to sync start each module This IOCTL doesn't configure any register and only enable pipeline to start processing.
|
inlinestatic |
Vhwa_M2mMscInitParams structure init function.
| mscInitPrms | Pointer to Vhwa_M2mMscInitParams structure. |
|
inlinestatic |
Function to initialize the MSC configuration parameters to default.
| mscCfg | Pointer to a Vhwa_M2mMscParams containing MSC configuration |
|
inlinestatic |
Function to initialize the MSC create params to default.
| createArgs | Pointer to a Vhwa_M2mMscCreatePrms, MSC Create Args |
| int32_t Vhwa_m2mMscInit | ( | const Vhwa_M2mMscInitParams * | initPrms | ) |
MSC initialization function. This function initializes the MSC hardware and drivers. This function should be called before calling any driver APIs and only once.
| initPrms | Pointer to a Vhwa_M2mMscInitParams structure containing the MSC driver initialization parameters |
| int32_t Vhwa_m2mMscDeInit | ( | void | ) |
MSC de-initialization function. This function un-initializes the MSC hardware and drivers. This function should be called during system shutdown if Vhwa_m2mMscDeInit() was called by the application.
| int32_t Vhwa_m2mMscAllocSl2 | ( | const Vhwa_M2mMscSl2AllocPrms * | sl2allocPrms | ) |
Function to allocate Sl2 memory for input and output buffers.
| sl2allocPrms | Pointer to a Vhwa_M2mMscSl2AllocPrms structure containing the SL2 allocation parameters |
| int32_t Vhwa_m2mMscFreeSl2 | ( | void | ) |
Function to free allocated SL2.
|
inlinestatic |