MCUSW
DIO Driver API

Introduction

The DIO Driver provides services for reading and writing to/from

This specification is applicable to drivers only for on chip DIO pins and ports
This module works on pins and ports which are configured by the PORT driver for this purpose.
For this reason, there is no configuration and initialization of this port structure in the DIO Driver

See also
DIO Configuration

Sub Modules

 DIO Configuration
 

Data Structures

struct  Dio_RegisterReadbackType
 

Macros

#define DIO_PORT_WIDTH   (32U)
 Width of GPIO register in this platform not to be modified. More...
 
#define DIO_MCAL_2139_FIXED   (0U)
 Read back issue in Maxwell is resolved or not. More...
 

DIO Driver Module SW Version Info

Defines for DIO Driver version used for compatibility checks

#define DIO_SW_MAJOR_VERSION   (3U)
 Driver Implementation Major Version. More...
 
#define DIO_SW_MINOR_VERSION   (0U)
 Driver Implementation Minor Version. More...
 
#define DIO_SW_PATCH_VERSION   (0U)
 Driver Implementation Patch Version. More...
 

DIO Driver Module AUTOSAR Version Info

Defines for DIO Driver AUTOSAR version used for compatibility checks

#define DIO_AR_RELEASE_MAJOR_VERSION   (4U)
 AUTOSAR Major version specification implemented by DIO Driver. More...
 
#define DIO_AR_RELEASE_MINOR_VERSION   (3U)
 AUTOSAR Minor version specification implemented by DIO Driver. More...
 
#define DIO_AR_RELEASE_REVISION_VERSION   (1U)
 AUTOSAR Patch version specification implemented by DIO Driver. More...
 

DIO Driver ID Info

#define DIO_VENDOR_ID   ((uint16) 44U)
 Texas Instruments Vendor ID. More...
 
#define DIO_MODULE_ID   ((uint16) 120U)
 DIO Driver Module ID. More...
 

Dio Error Codes

Error codes returned by Driver functions

#define DIO_E_PARAM_INVALID_CHANNEL_ID   (0x0AU)
 ERROR:API service called with invalid channel ID. More...
 
#define DIO_E_PARAM_INVALID_PORT_ID   (0x14U)
 ERROR:API service called with invalid port ID. More...
 
#define DIO_E_PARAM_INVALID_GROUP   (0x1FU)
 ERROR:API service called with invalid channel group ID. More...
 
#define DIO_E_PARAM_POINTER   (0x20U)
 ERROR:Dio_GetVersionInfo() called with NULL_PTR as parameter. More...
 

Dio Service Ids

The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error

#define DIO_SID_READ_CHANNEL   (0U)
 Dio_ReadChannel() More...
 
#define DIO_SID_WRITE_CHANNEL   (1U)
 Dio_WriteChannel() More...
 
#define DIO_SID_READ_PORT   (2U)
 Dio_ReadPort() More...
 
#define DIO_SID_WRITE_PORT   (3U)
 Dio_WritePort() More...
 
#define DIO_SID_READ_CHL_GROUP   (4U)
 Dio_ReadChannelGroup() More...
 
#define DIO_SID_WRITE_CHL_GROUP   (5U)
 Dio_WriteChannelGroup() More...
 
#define DIO_SID_FLIP_CHANNEL   (7U)
 Dio_FlipChannel() More...
 
#define DIO_SID_GET_VERSION_INFO   (18U)
 Dio_GetVersionInfo() More...
 

Macro Definition Documentation

◆ DIO_SW_MAJOR_VERSION

#define DIO_SW_MAJOR_VERSION   (3U)

Driver Implementation Major Version.

◆ DIO_SW_MINOR_VERSION

#define DIO_SW_MINOR_VERSION   (0U)

Driver Implementation Minor Version.

◆ DIO_SW_PATCH_VERSION

#define DIO_SW_PATCH_VERSION   (0U)

Driver Implementation Patch Version.

◆ DIO_AR_RELEASE_MAJOR_VERSION

#define DIO_AR_RELEASE_MAJOR_VERSION   (4U)

AUTOSAR Major version specification implemented by DIO Driver.

◆ DIO_AR_RELEASE_MINOR_VERSION

#define DIO_AR_RELEASE_MINOR_VERSION   (3U)

AUTOSAR Minor version specification implemented by DIO Driver.

◆ DIO_AR_RELEASE_REVISION_VERSION

#define DIO_AR_RELEASE_REVISION_VERSION   (1U)

AUTOSAR Patch version specification implemented by DIO Driver.

◆ DIO_VENDOR_ID

#define DIO_VENDOR_ID   ((uint16) 44U)

Texas Instruments Vendor ID.

◆ DIO_MODULE_ID

#define DIO_MODULE_ID   ((uint16) 120U)

DIO Driver Module ID.

◆ DIO_E_PARAM_INVALID_CHANNEL_ID

#define DIO_E_PARAM_INVALID_CHANNEL_ID   (0x0AU)

ERROR:API service called with invalid channel ID.

◆ DIO_E_PARAM_INVALID_PORT_ID

#define DIO_E_PARAM_INVALID_PORT_ID   (0x14U)

ERROR:API service called with invalid port ID.

◆ DIO_E_PARAM_INVALID_GROUP

#define DIO_E_PARAM_INVALID_GROUP   (0x1FU)

ERROR:API service called with invalid channel group ID.

◆ DIO_E_PARAM_POINTER

#define DIO_E_PARAM_POINTER   (0x20U)

ERROR:Dio_GetVersionInfo() called with NULL_PTR as parameter.

◆ DIO_SID_READ_CHANNEL

#define DIO_SID_READ_CHANNEL   (0U)

◆ DIO_SID_WRITE_CHANNEL

#define DIO_SID_WRITE_CHANNEL   (1U)

◆ DIO_SID_READ_PORT

#define DIO_SID_READ_PORT   (2U)

◆ DIO_SID_WRITE_PORT

#define DIO_SID_WRITE_PORT   (3U)

◆ DIO_SID_READ_CHL_GROUP

#define DIO_SID_READ_CHL_GROUP   (4U)

◆ DIO_SID_WRITE_CHL_GROUP

#define DIO_SID_WRITE_CHL_GROUP   (5U)

◆ DIO_SID_FLIP_CHANNEL

#define DIO_SID_FLIP_CHANNEL   (7U)

◆ DIO_SID_GET_VERSION_INFO

#define DIO_SID_GET_VERSION_INFO   (18U)

◆ DIO_PORT_WIDTH

#define DIO_PORT_WIDTH   (32U)

Width of GPIO register in this platform not to be modified.

◆ DIO_MCAL_2139_FIXED

#define DIO_MCAL_2139_FIXED   (0U)

Read back issue in Maxwell is resolved or not.