PDK API Guide for J721S2
|
ICSSG peripheral configuration parameters.
Data Fields | |
uint64_t | agingPeriod |
EnetPort_VlanCfg | vlanCfg |
const void * | dmaCfg |
EnetRm_ResCfg | resCfg |
Mdio_Cfg | mdioCfg |
IcssgTimeSync_Cfg | timeSyncCfg |
EnetMacPort_Interface | mii |
uint32_t | cycleTimeNs |
uint64_t Icssg_Cfg::agingPeriod |
FDB entry aging period
EnetPort_VlanCfg Icssg_Cfg::vlanCfg |
Default VLAN Id and PCP for port
const void* Icssg_Cfg::dmaCfg |
Configuration of the ICSSG DMA. Note - In Dual MAC mode, even though separate RX channel is opened for each port, same dmaCfg is used for both
EnetRm_ResCfg Icssg_Cfg::resCfg |
Configuration of the resource partition
Mdio_Cfg Icssg_Cfg::mdioCfg |
Configuration of the MDIO module
IcssgTimeSync_Cfg Icssg_Cfg::timeSyncCfg |
TimeSync configuration parameters
EnetMacPort_Interface Icssg_Cfg::mii |
MII mode for both MAC ports
uint32_t Icssg_Cfg::cycleTimeNs |
Cycle time in nanoseconds