PDK API Guide for J721S2
|
Port MAC mode configuration.
Data Fields | |
bool | macOnlyCafEn |
bool | macOnlyEn |
bool CpswAle_PortMacModeCfg::macOnlyCafEn |
MAC-only Copy All Frames:
bool CpswAle_PortMacModeCfg::macOnlyEn |
MAC-only. When set enables this port be treated like a MAC port for the host. All traffic received is only sent to the host. The host must direct traffic to this port as the lookup engine will not send traffic to the ports with the p0_maconly bit set and the p0_no_learn also set. If p0_maconly bit is set and the p0_no_learn is not set, the host can send non-directed packets that can be sent to the destination of a MacOnly port. It is also possible that The host can broadcast to ports including MacOnly ports in this mode