![]() |
PDK API Guide for J7200
|
This file contains the type definitions and helper macros for the Enet Trace interface.
Go to the source code of this file.
Macros | ||||||||||||||||||||||
Build-Time Trace Levels | ||||||||||||||||||||||
Enet LLD supports two types of trace levels: build-time and runtime. Build time trace level is specified via ENET_CFG_TRACE_LEVEL and can be any of the levels in this group. The runtime trace level is set through Enet_setTraceLevel(). The runtime trace level should be set equal to or less than the build-time trace level. | ||||||||||||||||||||||
| #define | ENET_CFG_TRACE_LEVEL_NONE (0U) | |||||||||||||||||||||
| All traces disabled at build-time. More... | ||||||||||||||||||||||
| #define | ENET_CFG_TRACE_LEVEL_ERROR (1U) | |||||||||||||||||||||
| Build-time error level. More... | ||||||||||||||||||||||
| #define | ENET_CFG_TRACE_LEVEL_WARN (2U) | |||||||||||||||||||||
| Build-time warning level. More... | ||||||||||||||||||||||
| #define | ENET_CFG_TRACE_LEVEL_INFO (3U) | |||||||||||||||||||||
| Build-time information level. More... | ||||||||||||||||||||||
| #define | ENET_CFG_TRACE_LEVEL_DEBUG (4U) | |||||||||||||||||||||
| Build-time debug level. More... | ||||||||||||||||||||||
| #define | ENET_CFG_TRACE_LEVEL_VERBOSE (5U) | |||||||||||||||||||||
| Build-time verbose level. More... | ||||||||||||||||||||||
Trace Formats | ||||||||||||||||||||||
The following trace formats are supported:
Any of these trace formats can also be prefixed with a timestamp. | ||||||||||||||||||||||
| #define | ENET_CFG_TRACE_FORMAT_FUNC (0U) | |||||||||||||||||||||
| Trace prefix: "<func>: string". More... | ||||||||||||||||||||||
| #define | ENET_CFG_TRACE_FORMAT_FILE (1U) | |||||||||||||||||||||
| Trace prefix: "<file>: <line>: string". More... | ||||||||||||||||||||||
| #define | ENET_CFG_TRACE_FORMAT_FULL (2U) | |||||||||||||||||||||
| Trace prefix: "<file>: <line>: <func>: string". More... | ||||||||||||||||||||||
| #define | ENET_CFG_TRACE_FORMAT_FUNC_TS (3U) | |||||||||||||||||||||
| Trace prefix: "<timestamp>: <func>: string". More... | ||||||||||||||||||||||
| #define | ENET_CFG_TRACE_FORMAT_FILE_TS (4U) | |||||||||||||||||||||
| Trace prefix: "<timestamp>: <file>: <line>: string". More... | ||||||||||||||||||||||
| #define | ENET_CFG_TRACE_FORMAT_FULL_TS (5U) | |||||||||||||||||||||
| Trace prefix: "<timestamp>: <file>: <line>: <func>: string". More... | ||||||||||||||||||||||
Enet Trace Configuration Parameters | ||||||||||||||||||||||
The default values of the Enet Trace configuration parameters if none is provided via enet_cfg.h. | ||||||||||||||||||||||
| #define | ENET_CFG_TRACE_LEVEL (ENET_CFG_TRACE_LEVEL_INFO) | |||||||||||||||||||||
| Default trace level if none is set. More... | ||||||||||||||||||||||
| #define | ENET_CFG_TRACE_FORMAT (ENET_CFG_TRACE_FORMAT_FUNC) | |||||||||||||||||||||
| Default trace format if none is specified. More... | ||||||||||||||||||||||
Enet Trace Error Code | ||||||||||||||||||||||
Enet Trace is capable of generating unique error codes from module id (Enet core, soc, per, mod, phy, etc), line number (where error code was reported) and status (error value reported by the module). The error code is a 32-bit value which is generated as follows:
Each individual source file in the locations shown in previous table is considered a module and is tagged with a unique | ||||||||||||||||||||||
| #define | ENET_TRACE_ERRCODE_MOD_OFFSET (20U) | |||||||||||||||||||||
| Module id offset in the error code value. More... | ||||||||||||||||||||||
| #define | ENET_TRACE_ERRCODE_MOD_MAJ_OFFSET (28U) | |||||||||||||||||||||
| Module id (major number) offset in the error code value. More... | ||||||||||||||||||||||
| #define | ENET_TRACE_ERRCODE_MOD_MIN_OFFSET (20U) | |||||||||||||||||||||
| Module id (minor number) offset in the error code value. More... | ||||||||||||||||||||||
| #define | ENET_TRACE_ERRCODE_LINE_OFFSET (8U) | |||||||||||||||||||||
| Line number offset in the error code value. More... | ||||||||||||||||||||||
| #define | ENET_TRACE_ERRCODE_STATUS_OFFSET (0U) | |||||||||||||||||||||
| Status offset in the error code value. More... | ||||||||||||||||||||||
| #define | ENET_TRACE_ERRCODE_MOD_MASK (0xFFF00000U) | |||||||||||||||||||||
| Module id mask in the error code value. More... | ||||||||||||||||||||||
| #define | ENET_TRACE_ERRCODE_MOD_MAJ_MASK (0xF0000000U) | |||||||||||||||||||||
| Module id (major number) mask in the error code value. More... | ||||||||||||||||||||||
| #define | ENET_TRACE_ERRCODE_MOD_MIN_MASK (0x0FF00000U) | |||||||||||||||||||||
| Module id (minor number) mask in the error code value. More... | ||||||||||||||||||||||
| #define | ENET_TRACE_ERRCODE_LINE_MASK (0x000FFF00U) | |||||||||||||||||||||
| Line number mask in the error code value. More... | ||||||||||||||||||||||
| #define | ENET_TRACE_ERRCODE_STATUS_MASK (0x000000FFU) | |||||||||||||||||||||
| Status mask in the error code value. More... | ||||||||||||||||||||||
| #define | ENET_TRACE_ERRCODE_MOD(x) | |||||||||||||||||||||
| Helper macro to extract the module id from the error code value. More... | ||||||||||||||||||||||
| #define | ENET_TRACE_ERRCODE_MOD_MAJ(x) | |||||||||||||||||||||
| Helper macro to extract the module id (major number) from the error code value. More... | ||||||||||||||||||||||
| #define | ENET_TRACE_ERRCODE_MOD_MIN(x) | |||||||||||||||||||||
| Helper macro to extract the module id (minor number) from the error code value. More... | ||||||||||||||||||||||
| #define | ENET_TRACE_ERRCODE_LINE(x) | |||||||||||||||||||||
| Helper macro to extract the line number from the error code value. More... | ||||||||||||||||||||||
| #define | ENET_TRACE_ERRCODE_STATUS(x) | |||||||||||||||||||||
| Helper macro to extract the status value from the error code value. More... | ||||||||||||||||||||||
Typedefs | |
| typedef uint64_t(* | EnetTrace_TraceTsFunc) (void) |
| Callback function used to get trace timestamps. More... | |
| typedef void(* | EnetTrace_ExtTraceFunc) (uint32_t errCode) |
| Callback function called to report errors. More... | |
Enumerations | |
| enum | EnetTrace_TraceLevel { ENET_TRACE_NONE = 0U, ENET_TRACE_ERROR = 1U, ENET_TRACE_WARN = 2U, ENET_TRACE_INFO = 3U, ENET_TRACE_DEBUG = 4U, ENET_TRACE_VERBOSE = 5U } |
| Enumerates the types of trace level. More... | |