![]() |
PDK API Guide for J7200
|
Timer interface for the RTOS Porting Interface.
============================================================================
The TimerP module can be used to create a timer (that is, to mark a timer for use) and configure it to call a tickFxn when the timer expires.
The timer can be configured as a one-shot or a continuous mode timer. The period can be specified in timer counts or microseconds. The timer interrupt always uses the Hwi dispatcher. The Timer tickFxn runs in the context of a Hwi thread. The Timer module automatically creates a
Go to the source code of this file.
Timer period units for TimerP APIs | |
| #define | TimerP_PeriodType_MICROSECS ( (uint32_t) 0U) |
| #define | TimerP_PeriodType_COUNTS ( (uint32_t) 1U) |
| typedef uint32_t | TimerP_PeriodType |
| This enumerator defines the Timer Period unit. More... | |
Timer runtime modes for TimerP APIs | |
| #define | TimerP_RunMode_CONTINUOUS ( (uint32_t) 0U) |
| #define | TimerP_RunMode_ONESHOT ( (uint32_t) 1U) |
| typedef uint32_t | TimerP_RunMode |
| This enumerator defines the Timer runtime modes. More... | |
Timer start modes for TimerP APIs | |
| #define | TimerP_StartMode_AUTO ( (uint32_t) 0U) |
| #define | TimerP_StartMode_USER ( (uint32_t) 1U) |
| typedef uint32_t | TimerP_StartMode |
| This enumerator defines the Timer start modes. More... | |
Data Structures | |
| struct | TimerP_FreqHz |
| Frequency-in-hertz struct. More... | |
| struct | TimerP_Params |
| Basic TimerP Parameters. More... | |
Macros | |
| #define | TimerP_ANY ((uint32_t)0xFEEDU) |
| #define | TimerP_ANY_MAX_RESTRICTIONS ((uint32_t)15U) |
| #define | TimerP_ID_INVALID ((uint32_t)0xFFFFU) |
| #define | TimerP_MAX_PERIOD ((uint32_t)0xFFFFFFFFU) |
| #define | TimerP_USE_DEFAULT ((uint32_t)0xFFFFFFFFU) |
Typedefs | |
| typedef void * | TimerP_Handle |
| Opaque client reference to an instance of a TimerP. More... | |
| typedef void(* | TimerP_Fxn) (uintptr_t arg) |
| Prototype for a TimerP function. More... | |
Enumerations | |
| enum | TimerP_Status { TimerP_OK = 0, TimerP_FAILURE = (-(int32_t) 1), TimerP_NOT_AVAILABLE = (-(int32_t) 2), TimerP_BAD_INT_NUM = (-(int32_t) 3), TimerP_ISR_HOOK_ERR = (-(int32_t) 4) } |
| Status codes for TimerP APIs. More... | |
| enum | TimerP_Timer64Mode { TimerP_Timer64Mode_64BITGPTIMER, TimerP_Timer64Mode_UNCHAINED, TimerP_Timer64Mode_CHAINED } |
| Timer mode for 64 bit timers (KeyStone devices) More... | |
| enum | TimerP_Timer64Half { TimerP_Timer64Half_LOWER, TimerP_Timer64Half_UPPER, TimerP_Timer64Half_DEFAULT } |
| Timer half when 64 bit timer is split into two 32 bit timer (Keystone devices) More... | |
Functions | |
| TimerP_Handle | TimerP_create (uint32_t id, TimerP_Fxn tickFxn, const TimerP_Params *timerParams) |
| Function to create a timer object. More... | |
| TimerP_Status | TimerP_delete (TimerP_Handle timerHandle) |
| Function to delete a timer. More... | |
| TimerP_Status | TimerP_setPeriodMicroSecs (TimerP_Handle timerHandle, uint32_t microsecs) |
| Function to set timer period specified in micro seconds A best-effort method will be used to set the period register. There might be a slight rounding error based on resolution of timer period register. If the timer frequency cannot support the requested period, i.e. the timer period register cannot support the requested period, then this function returns false. TimerP_setPeriodMicroSecs() invokes TimerP_stop() prior to setting the period and leaves the timer in the stopped state. More... | |
| void | TimerP_Params_init (TimerP_Params *timerParams) |
| Initialize params structure to default values. More... | |
| TimerP_Status | TimerP_start (TimerP_Handle timerHandle) |
| Function to start a timer. More... | |
| TimerP_Status | TimerP_stop (TimerP_Handle timerHandle) |
| Function to stop a timer. More... | |
| TimerP_Status | TimerP_ClearInterrupt (TimerP_Handle timerHandle) |
| Function to clear the interrupt of the timer. More... | |
| uint64_t | TimerP_getTimeInUsecs (void) |
| Function to return current time in units of micro-secs. More... | |
| uint32_t | TimerP_getReloadCount (TimerP_Handle timerHandle) |
| Get timer reload count. More... | |
| uint32_t | TimerP_getCount (TimerP_Handle timerHandle) |
| Get timer current count. More... | |