2.2. Release Notes - 08_04_00¶
2.2.1. Introduction¶
This release notes provides important information that will assist you in using the PDK software package for the Jacinto family of devices. This document provides the product information and known issues that are specific to the PDK software package.
New features added / supported is listed below and defects fixed are highlighted in Fixed Issues. Also please check Upgrade and Compatibility for backward compatibility
2.2.2. What’s New¶
ID | Description | Module | Supported Platforms |
---|---|---|---|
PDK-10132 | J7VCL DDR Init Time Further Optimizations | BOARD | J7200 |
PDK-12191 | SafeRTOS Support on R5F for CPU | OSAL | J7200 |
2.2.3. Upgrade and Compatibility¶
2.2.3.1. SBL¶
- We have modified the CPU IDs for all cores due to an increase in the number of cores in latest Jacinto device. E.g. CPU Id of mcu1_0 has been updated from 4 to 8.
- Hence user needs to generate the new app image with the current release to use the latest SBL.
- CPU IDs corresponding to each core can be found here: <pdk_base>/packages/ti/build/makerules/platform.mk.
2.2.3.2. SPI¶
- Previously SPI_open supported only 5 instances of McSPI(3 MCU instances and 2 Main Instances). Now separate APIs are implemented for McSPI and OSPI in order to support all the instances, user needs to use specific APIs as per the peripheral. E.g. User should use SPI_open() for McSPI and OSPI_open() for OSPI.
2.2.3.3. FreeRTOS¶
- On C66x CPU, interrupt router configurations for OS ticks is now handled in the OS_init() by FreeRTOS OSAL layer. Previously this configuration was done by application which is no longer needed.
2.2.4. Device Support¶
J7200 GP SR1.0 and SR2.0, J7200-HS SR1.0 and SR 2.0 (BOARD=j7200_evm)
Associated TIFS versions:
TIFS name J7200 SR revision tifs.bin SR1.0 GP & SR 2.0 GP tifs-hs-enc.bin SR1.0 HS tifs_sr2-hs-enc.bin SR2.0 HS
2.2.5. Validation Information¶
For details on the validated examples refer to the platform specific test report available here.
2.2.6. Tool Chain Information¶
Component | Version |
---|---|
FreeRTOS Kernel | 10.4.3 |
lwIP stack | 2.1.2 |
lwIP-contrib | 2.1.0 |
TI ARM CLANG | 1.3.0.LTS |
PRU code generation tools | 2.3.3 |
GCC ARM code generation tools | ARCH64 9.2-2019.12 |
CGT XML Processing Scripts | 2.61.00 |
System Analyzer (UIA Target) | 2_30_01_02 |
2.2.7. Change Request¶
ID | Head Line | Original Fix Version | New Fix Version |
---|---|---|---|
NA | NA | NA | NA |
2.2.8. Fixed Issues¶
ID | Head Line | Module | Affected Versions | Affected Platforms |
---|---|---|---|---|
PDK-10139 | J7200 App load on MCU R5_1 core may fail with CCS boot flow | COMMON | 08.00.00 | J7200 |
PDK-11152 | SPI driver does not support all instances with SPI_open | McSPI | 08.02.00 | J721E, J7200 |
PDK-11388 | [SBL] SBL should not copy build folder contents to board folder during packaging | SBL | 08.01.00 | J721E, J7200 |
PDK-11093 | ACK/NACK is send for TISCI messages without AOP flag | Sciclient | 08.01.00 | J721E, J7200 |
PDK-11227 | UART instances 3-9 does not work on MAIN R5 in interrupt mode | UART | 08.01.00 | J721E, J7200, J721S2 |
PDK-11861 | Unable to program PVU | CSL | 08.02.00 | J721E, J7200 |
PDK-11975 | OCMC RAM used by Sciserver FreeRTOS Testapp may cause memory conflict | SCICLIENT | 08.02.00 | J721E, J7200, J721S2 |
2.2.9. Known Issues¶
ID | Head Line | Module | Reported in Release | Affected Platforms | Impact | Workaround in this release |
---|---|---|---|---|---|---|
PDK-6975 | Pulsar (R5F) : High priority interrupt is missed by VIM | CSL, OSAL | 07.00.00 | J721E, J7200 | Baremetal implementation is pending | Use RTOS instead of baremetal |
PDK-9676 | UART : Potential interrupt storm | UART | 07.02.00 | J721E, J7200 | Error interrupt resulting in hang. | None |
PDK-8601 | CSL ECC test application fails on J7200/J721S2 | CSL | 07.01.00 | J7200, J721S2 | None | None |
PDK-10128 | Spi_AsyncTransmit can not transmit more than 32 bytes | McSPI | 07.03.00 | J7200 | None | None |
PDK-10925 | IPC Performance Test hangs after loading the binary | IPC | 08.01.00 | J721E, J7200 | The app won’t work for this release | None |
PDK-11085 | SPI instance should be decided by SPI driver and not Board Module | OSPI | 08.01.00 | J721E, J7200 | None | None |
PDK-11240 | keywriter: smek gets generated even when argument not specified | Security | 08.01.00 | J721E, J7200 | None | None |
PDK-11854 | USART: Spurious DMA Interrupts | UART | 08.04.00 | J721E, J7200, J721S2 | None | None |
PDK-11973 | USART: Erroneous clear/trigger of timeout interrupt | UART | 08.02.00 | J721E, J7200, J721S2 | None | None |
PDK-12060 | Main Domain GPIO does not service interrupts | GPIO | 08.04.00 | J721E, J7200 | None | None |
PDK-12107 | DM: UART Traces are not working with Linux SDK | PM | 08.02.00 | J721E, J7200 | None | None |
PDK-12164 | Incorrect DDR End Address with ECC enabled | BOARD | 08.02.00 | J721E, J7200 | None | None |
PDK-12153 | DDR ECC example: returned error address incorrectly shifted | CSL | 08.02.00 | J7200 | None | None |
2.2.10. Limitations¶
2.2.10.1. PDK¶
- PDK examples do not support SMP mode. Some of examples still support build in SMP mode but these binaries are not supported or validated.
- TI Clang compiler does not enable O3 optimization level and Thumb2 mode which were enabled by default with TI ARM CGT compiler. This has an impact on driver throughput. E.g. Ethernet performance has reduced by ~20% on J7200
2.2.10.2. ENET¶
- lwIP stack integration doesn’t support checksum hardware-offload feature.