PDK API Guide for J7200
|
Input args for ENET_MDIO_IOCTL_C22_WRITE command.
Clause-22 register write arguments.
Data Fields | |
EnetMdio_Group | group |
uint8_t | phyAddr |
uint16_t | reg |
uint16_t | val |
EnetMdio_Group EnetMdio_C22WriteInArgs::group |
User channel to be used to perform the register access
uint8_t EnetMdio_C22WriteInArgs::phyAddr |
PHY address
uint16_t EnetMdio_C22WriteInArgs::reg |
Register address
uint16_t EnetMdio_C22WriteInArgs::val |
Value to be written