MCUSW
|
Mode info type.
Data Fields | |
uint32 | reaction |
uint32 | windowSize |
uint32 | timeOutVal |
uint32 Wdg_ModeInfoType::reaction |
Reaction type 0x5 - This value causes a reset if the watchdog is serviced outside the time window defined by the configuration, or if the watchdog is not serviced at all. 0xA - The windowed watchdog will generate a non-maskable interrupt to the CPU if the watchdog is serviced outside the time window defined by the configuration, or if the watchdog is not serviced at all.
uint32 Wdg_ModeInfoType::windowSize |
Different Window Sizes Refer Watchdog Window Size section above for different Window sizes
uint32 Wdg_ModeInfoType::timeOutVal |
Watchdog timeout value in milli seconds