MCUSW
|
Defines Shared Memories for VRING and VRING OBJECT VRING is the shared memory between cores and VRING OBJECT is used implement queue. Please refer design/user guide for details.
Data Fields | |
void * | vertIoRingAddr |
uint32 | vertIoRingSize |
uint32 | vertIoObjSize |
uint32 | reserved |
void* Cdd_IpcVertIoType::vertIoRingAddr |
Defines address that shall be shared between cores
uint32 Cdd_IpcVertIoType::vertIoRingSize |
Size of the shared memory
uint32 Cdd_IpcVertIoType::vertIoObjSize |
Size of the vertio Object, used for vertIoRing
uint32 Cdd_IpcVertIoType::reserved |
Future use if any