![]() |
MCUSW
|
Defines logical communication channel between cores.
Data Fields | |
uint32 | id |
uint32 | localEp |
uint32 | remoteEp |
uint32 | remoteProcId |
uint32 | numMsgQueued |
uint32 | maxMsgSize |
uint32 | reserved |
uint32 Cdd_IpcChannelType::id |
Unique identifiers for a channel
uint32 Cdd_IpcChannelType::localEp |
Local End Point identifier, on which MCAL/AUTOSAR is hosted
uint32 Cdd_IpcChannelType::remoteEp |
Remote End Point identifier, on remote cores
uint32 Cdd_IpcChannelType::remoteProcId |
Remote Processor Identifier
uint32 Cdd_IpcChannelType::numMsgQueued |
Maximum depth of the queue, that holds received messages
uint32 Cdd_IpcChannelType::maxMsgSize |
Maximum size of the message that could be received
uint32 Cdd_IpcChannelType::reserved |
Future use if any