![]() |
MCUSW
|
Structure defining the CAN FD data phase baud rate configuration.
Data Fields | |
uint16 | Baud |
uint8 | PropSeg |
uint8 | Pseg1 |
uint8 | Pseg2 |
uint8 | Sjw |
uint16 | TimingValues |
uint16 | BrpValue |
uint16 | TrcvCompDelay |
boolean | BrsSwitch |
uint16 Can_FdBaudConfigType::Baud |
In Kbps
uint8 Can_FdBaudConfigType::PropSeg |
Prop Segement value
uint8 Can_FdBaudConfigType::Pseg1 |
Phase Segment 1
uint8 Can_FdBaudConfigType::Pseg2 |
Phase Segment 2
uint8 Can_FdBaudConfigType::Sjw |
Sync jump width
uint16 Can_FdBaudConfigType::TimingValues |
Sum of all timing parameters *
uint16 Can_FdBaudConfigType::BrpValue |
Controller BRP value for Baud
uint16 Can_FdBaudConfigType::TrcvCompDelay |
Specifies the Transceiver Delay Compensation Offset in ns
boolean Can_FdBaudConfigType::BrsSwitch |
Specifies if the bit rate switching shall be used for transmissions.