MCUSW
|
Can MCAL root configuration structure.
Data Fields | |
Can_ControllerType ** | CanControllerList |
uint8 | CanMaxControllerCount |
Can_MailboxType ** | MailBoxList |
uint32 | MaxMbCnt |
uint32 | MaxBaudConfigID [CAN_MAX_CONTROLLER] |
Can_DmaPrms * | DmaPrms |
Can_ControllerType** Can_ConfigType::CanControllerList |
List of enabled Controllers
uint8 Can_ConfigType::CanMaxControllerCount |
MaxCount of Controller in Controller List
Can_MailboxType** Can_ConfigType::MailBoxList |
MB array for all controllers
uint32 Can_ConfigType::MaxMbCnt |
MaxMbCount in MB list in all controller
uint32 Can_ConfigType::MaxBaudConfigID[CAN_MAX_CONTROLLER] |
Max Baud Config Index in BaudRateConfigList in all controller
Can_DmaPrms* Can_ConfigType::DmaPrms |
Reserved for Future use, currently unused parameter