![]() |
MCUSW
|
ADC log structure per group entry.
Data Fields | |
uint32 | timeStamp |
Adc_GroupType | groupId |
Adc_HWUnitType | hwUnitId |
uint32 | isReScheduled |
uint32 Adc_GroupLogEntryType::timeStamp |
Timestamp based on 32-kHz Synchronized Timer (COUNTER_32K) at which the group is scheduled
Adc_GroupType Adc_GroupLogEntryType::groupId |
Group ID of the scheduled group
Adc_HWUnitType Adc_GroupLogEntryType::hwUnitId |
HWUnit associated with the group
uint32 Adc_GroupLogEntryType::isReScheduled |
This will be set to TRUE is a group is rescheduled when a higher priority task pre-empts this group