![]() |
MCUSW
|
This component provides services for initialization and control of the ICU unit. The ICU module captures and measures signals. signal period time.
Sub Modules | |
ICU Configuration | |
ICU Driver Interrupt Handlers | |
ICU Driver ID Info | |
#define | ICU_VENDOR_ID ((uint16) 44U) |
Texas Instruments Vendor ID. More... | |
#define | ICU_MODULE_ID ((uint16) 122U) |
ICU Driver Module ID. More... | |
#define | ICU_INSTANCE_ID ((uint8) 0U) |
ICU Driver Instance ID. More... | |
ICU Driver Module SW Version Info | |
Defines for ICU Driver version used for compatibility checks | |
#define | ICU_SW_MAJOR_VERSION (2U) |
Driver Implementation Major Version. More... | |
#define | ICU_SW_MINOR_VERSION (0U) |
Driver Implementation Minor Version. More... | |
#define | ICU_SW_PATCH_VERSION (0U) |
Driver Implementation Patch Version. More... | |
ICU Driver Module AUTOSAR Version Info | |
Defines for ICU Driver AUTOSAR version used for compatibility checks | |
#define | ICU_AR_RELEASE_MAJOR_VERSION (4U) |
AUTOSAR Major version specification implemented by ICU Driver. More... | |
#define | ICU_AR_RELEASE_MINOR_VERSION (3U) |
AUTOSAR Minor version specification implemented by ICU Driver. More... | |
#define | ICU_AR_RELEASE_REVISION_VERSION (1U) |
AUTOSAR Patch version specification implemented by ICU Driver. More... | |
ICU Service IDs | |
The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error | |
#define | ICU_INIT_ID ((uint8) 0x00U) |
Icu_Init() API Service ID. More... | |
#define | ICU_DEINIT_ID ((uint8) 0x01U) |
Icu_DeInit() API Service ID. More... | |
#define | ICU_SETMODE_ID ((uint8) 0x02U) |
Icu_SetMode() API Service ID. More... | |
#define | ICU_SETACTIVATIONCONDITION_ID ((uint8) 0x05U) |
Icu_SetActivationCondition() API Service ID. More... | |
#define | ICU_DISABLENOTIFICATION_ID ((uint8) 0x06U) |
Icu_DisableNotification() API Service ID. More... | |
#define | ICU_ENABLENOTIFICATION_ID ((uint8) 0x07U) |
Icu_EnableNotification() API Service ID. More... | |
#define | ICU_GETINPUTSTATE_ID ((uint8) 0x08U) |
Icu_GetInputState() API Service ID. More... | |
#define | ICU_STARTTIMESTAMP_ID ((uint8) 0x09U) |
Icu_StartTimestamp() API Service ID. More... | |
#define | ICU_STOPTIMESTAMP_ID ((uint8) 0x0AU) |
Icu_StopTimestamp() API Service ID. More... | |
#define | ICU_GETTIMESTAMPINDEX_ID ((uint8) 0x0BU) |
Icu_GetTimeStampIndex() API Service ID. More... | |
#define | ICU_RESETEDGECOUNT_ID ((uint8) 0x0CU) |
Icu_ResetEdgeCount() API Service ID. More... | |
#define | ICU_ENABLEEDGECOUNT_ID ((uint8) 0x0DU) |
Icu_EnableEdgeCount() API Service ID. More... | |
#define | ICU_ENABLEEDGEDETECTION_ID ((uint8) 0x16U) |
Icu_EnableEdgeDetection() API Service ID. More... | |
#define | ICU_DISABLEEDGEDETECTION_ID ((uint8) 0x17U) |
Icu_DisableEdgeDetection() API Service ID. More... | |
#define | ICU_DISABLEEDGECOUNT_ID ((uint8) 0x0EU) |
Icu_DisableEdgeCount() API Service ID. More... | |
#define | ICU_GETEDGENUMBERS_ID ((uint8) 0x0FU) |
Icu_GetEdgeNumbers() API Service ID. More... | |
#define | ICU_STARTSIGNALMEASUREMENT_ID ((uint8) 0x13U) |
Icu_StartSignalMeasurement() API Service ID. More... | |
#define | ICU_STOPSIGNALMEASUREMENT_ID ((uint8) 0x14U) |
Icu_StopSignalMeasurement() API Service ID. More... | |
#define | ICU_GETTIMEELAPSED_ID ((uint8) 0x10U) |
Icu_GetTimeElapsed() API Service ID. More... | |
#define | ICU_GETDUTYCYCLEVALUES_ID ((uint8) 0x11U) |
Icu_GetDutyCycleValues() API Service ID. More... | |
#define | ICU_GETVERSIONINFO_ID ((uint8) 0x12U) |
Icu_GetVersionInfo() API Service ID. More... | |
ICU Error Codes | |
#define | ICU_E_PARAM_POINTER ((uint8) 0x0AU) |
API service called with invalid pointer. More... | |
#define | ICU_E_PARAM_CHANNEL ((uint8) 0x0BU) |
API service called with invalid channel identifier or channel not configured. More... | |
#define | ICU_E_PARAM_ACTIVATION ((uint8) 0x0CU) |
API service calleed with an invalid or not feasible activation. More... | |
#define | ICU_E_INIT_FAILED ((uint8) 0x0DU) |
Init Function Failed. More... | |
#define | ICU_E_PARAM_BUFFER_SIZE ((uint8) 0x0EU) |
API service used with invalid Buffer size. More... | |
#define | ICU_E_PARAM_MODE ((uint8) 0x0FU) |
API service called with invalid mode. More... | |
#define | ICU_E_UNINIT ((uint8) 0x14U) |
API service calleed without module initialisation. More... | |
#define | ICU_E_NOT_STARTED ((uint8) 0x16U) |
Icu_StopTimestamp called on channel not started or already stopped. More... | |
#define | ICU_E_BUSY_OPERATION ((uint8) 0x16U) |
API service called while a running operation. More... | |
#define | ICU_E_ALREADY_INITIALIZED ((uint8) 0x17U) |
API service Icu_Init called when module already initialized. More... | |
#define | ICU_E_PARAM_NOTIFY_INTERVAL ((uint8) 0x18U) |
API service called when notify interval is invalid. More... | |
#define | ICU_E_PARAM_VINFO ((uint8) 0x19U) |
API service Icu_GetVersionInfo called and parameter is invalid. More... | |
ICU Driver State Values | |
#define | ICU_STATUS_UNINIT ((uint8)(0U)) |
ICU driver Status uninitialized. More... | |
#define | ICU_STATUS_INIT ((uint8)(1U)) |
ICU driver Status Initialized. More... | |
Macros to define Rising and Falling edge config for capture registers | |
#define | ICU_FALLING ((uint8)(0U)) |
Capture regsiter configuration for FALLING edge. More... | |
#define | ICU_RISING ((uint8)(1U)) |
Capture regsiter configuration for RISING edge. More... | |
enum | Icu_ModeType { ICU_MODE_NORMAL, ICU_MODE_SLEEP } |
This type defines a range of mode type. More... | |
enum | Icu_InputStateType { ICU_ACTIVE, ICU_IDLE } |
This type defines a input state of ICU driver. More... | |
enum | Icu_ActivationType { ICU_RISING_EDGE, ICU_FALLING_EDGE, ICU_BOTH_EDGES } |
This type defines Activation range. More... | |
enum | Icu_MeasurementModeType { ICU_MODE_SIGNAL_EDGE_DETECT, ICU_MODE_SIGNAL_MEASUREMENT, ICU_MODE_TIMESTAMP, ICU_MODE_EDGE_COUNTER } |
This type defines available measurement modes. More... | |
enum | Icu_SignalMeasurementPropertyType { ICU_LOW_TIME, ICU_HIGH_TIME, ICU_PERIOD_TIME, ICU_DUTY_CYCLE } |
This type defines Signal Measurement Property range. More... | |
enum | Icu_TimestampBufferType { ICU_LINEAR_BUFFER, ICU_CIRCULAR_BUFFER } |
This type defines TimeStamp Property range. More... | |
typedef uint32 | Icu_ValueType |
This type defines Value type. More... | |
typedef uint32 | Icu_IndexType |
This type defines return value Icu_GetTimeStampIndex. More... | |
typedef uint32 | Icu_EdgeNumberType |
This type defines return value of Icu-Icu_GetEdgeNumbers. More... | |
typedef void(* | Icu_NotifyFuncType) (void) |
Notification callback function pointer. More... | |
typedef uint8 | Icu_ChannelType |
This type defines Channel type. More... | |
typedef uint32 | Icu_ChannelPrescalerType |
This type defines Prescaler type. More... | |
#define ICU_VENDOR_ID ((uint16) 44U) |
Texas Instruments Vendor ID.
#define ICU_MODULE_ID ((uint16) 122U) |
ICU Driver Module ID.
#define ICU_INSTANCE_ID ((uint8) 0U) |
ICU Driver Instance ID.
#define ICU_SW_MAJOR_VERSION (2U) |
Driver Implementation Major Version.
#define ICU_SW_MINOR_VERSION (0U) |
Driver Implementation Minor Version.
#define ICU_SW_PATCH_VERSION (0U) |
Driver Implementation Patch Version.
#define ICU_AR_RELEASE_MAJOR_VERSION (4U) |
AUTOSAR Major version specification implemented by ICU Driver.
#define ICU_AR_RELEASE_MINOR_VERSION (3U) |
AUTOSAR Minor version specification implemented by ICU Driver.
#define ICU_AR_RELEASE_REVISION_VERSION (1U) |
AUTOSAR Patch version specification implemented by ICU Driver.
#define ICU_INIT_ID ((uint8) 0x00U) |
Icu_Init() API Service ID.
#define ICU_DEINIT_ID ((uint8) 0x01U) |
Icu_DeInit() API Service ID.
#define ICU_SETMODE_ID ((uint8) 0x02U) |
Icu_SetMode() API Service ID.
#define ICU_SETACTIVATIONCONDITION_ID ((uint8) 0x05U) |
Icu_SetActivationCondition() API Service ID.
#define ICU_DISABLENOTIFICATION_ID ((uint8) 0x06U) |
Icu_DisableNotification() API Service ID.
#define ICU_ENABLENOTIFICATION_ID ((uint8) 0x07U) |
Icu_EnableNotification() API Service ID.
#define ICU_GETINPUTSTATE_ID ((uint8) 0x08U) |
Icu_GetInputState() API Service ID.
#define ICU_STARTTIMESTAMP_ID ((uint8) 0x09U) |
Icu_StartTimestamp() API Service ID.
#define ICU_STOPTIMESTAMP_ID ((uint8) 0x0AU) |
Icu_StopTimestamp() API Service ID.
#define ICU_GETTIMESTAMPINDEX_ID ((uint8) 0x0BU) |
Icu_GetTimeStampIndex() API Service ID.
#define ICU_RESETEDGECOUNT_ID ((uint8) 0x0CU) |
Icu_ResetEdgeCount() API Service ID.
#define ICU_ENABLEEDGECOUNT_ID ((uint8) 0x0DU) |
Icu_EnableEdgeCount() API Service ID.
#define ICU_ENABLEEDGEDETECTION_ID ((uint8) 0x16U) |
Icu_EnableEdgeDetection() API Service ID.
#define ICU_DISABLEEDGEDETECTION_ID ((uint8) 0x17U) |
Icu_DisableEdgeDetection() API Service ID.
#define ICU_DISABLEEDGECOUNT_ID ((uint8) 0x0EU) |
Icu_DisableEdgeCount() API Service ID.
#define ICU_GETEDGENUMBERS_ID ((uint8) 0x0FU) |
Icu_GetEdgeNumbers() API Service ID.
#define ICU_STARTSIGNALMEASUREMENT_ID ((uint8) 0x13U) |
Icu_StartSignalMeasurement() API Service ID.
#define ICU_STOPSIGNALMEASUREMENT_ID ((uint8) 0x14U) |
Icu_StopSignalMeasurement() API Service ID.
#define ICU_GETTIMEELAPSED_ID ((uint8) 0x10U) |
Icu_GetTimeElapsed() API Service ID.
#define ICU_GETDUTYCYCLEVALUES_ID ((uint8) 0x11U) |
Icu_GetDutyCycleValues() API Service ID.
#define ICU_GETVERSIONINFO_ID ((uint8) 0x12U) |
Icu_GetVersionInfo() API Service ID.
#define ICU_E_PARAM_POINTER ((uint8) 0x0AU) |
API service called with invalid pointer.
#define ICU_E_PARAM_CHANNEL ((uint8) 0x0BU) |
API service called with invalid channel identifier or channel not configured.
#define ICU_E_PARAM_ACTIVATION ((uint8) 0x0CU) |
API service calleed with an invalid or not feasible activation.
#define ICU_E_INIT_FAILED ((uint8) 0x0DU) |
Init Function Failed.
#define ICU_E_PARAM_BUFFER_SIZE ((uint8) 0x0EU) |
API service used with invalid Buffer size.
#define ICU_E_PARAM_MODE ((uint8) 0x0FU) |
API service called with invalid mode.
#define ICU_E_UNINIT ((uint8) 0x14U) |
API service calleed without module initialisation.
#define ICU_E_NOT_STARTED ((uint8) 0x16U) |
Icu_StopTimestamp called on channel not started or already stopped.
#define ICU_E_BUSY_OPERATION ((uint8) 0x16U) |
API service called while a running operation.
#define ICU_E_ALREADY_INITIALIZED ((uint8) 0x17U) |
API service Icu_Init called when module already initialized.
#define ICU_E_PARAM_NOTIFY_INTERVAL ((uint8) 0x18U) |
API service called when notify interval is invalid.
#define ICU_E_PARAM_VINFO ((uint8) 0x19U) |
API service Icu_GetVersionInfo called and parameter is invalid.
#define ICU_STATUS_UNINIT ((uint8)(0U)) |
ICU driver Status uninitialized.
#define ICU_STATUS_INIT ((uint8)(1U)) |
ICU driver Status Initialized.
#define ICU_FALLING ((uint8)(0U)) |
Capture regsiter configuration for FALLING edge.
#define ICU_RISING ((uint8)(1U)) |
Capture regsiter configuration for RISING edge.
typedef uint32 Icu_ValueType |
This type defines Value type.
typedef uint32 Icu_IndexType |
This type defines return value Icu_GetTimeStampIndex.
typedef uint32 Icu_EdgeNumberType |
This type defines return value of Icu-Icu_GetEdgeNumbers.
typedef void(* Icu_NotifyFuncType) (void) |
Notification callback function pointer.
typedef uint8 Icu_ChannelType |
This type defines Channel type.
typedef uint32 Icu_ChannelPrescalerType |
This type defines Prescaler type.
enum Icu_ModeType |
enum Icu_InputStateType |
enum Icu_ActivationType |