137 #include "WdgIf_Types.h" 158 #define WDG_SW_MAJOR_VERSION (2U) 160 #define WDG_SW_MINOR_VERSION (0U) 162 #define WDG_SW_PATCH_VERSION (0U) 172 #define WDG_AR_RELEASE_MAJOR_VERSION (4U) 174 #define WDG_AR_RELEASE_MINOR_VERSION (3U) 176 #define WDG_AR_RELEASE_REVISION_VERSION (1U) 184 #define WDG_VENDOR_ID ((uint16) 44U) 186 #define WDG_MODULE_ID ((uint16) 102U) 188 #define WDG_INSTANCE_ID ((uint8) 0U) 201 #define WDG_E_DRIVER_STATE ((uint8) 0x10U) 203 #define WDG_E_PARAM_MODE ((uint8) 0x11U) 205 #define WDG_E_PARAM_CONFIG ((uint8) 0x12U) 207 #define WDG_E_PARAM_TIMEOUT ((uint8) 0x13U) 209 #define WDG_E_PARAM_POINTER ((uint8) 0x14U) 211 #define WDG_E_INIT_FAILED ((uint8) 0x15U) 225 #define WDG_API_INIT ((uint8) 0x00U) 227 #define WDG_API_SET_MODE ((uint8) 0x01U) 229 #define WDG_SET_TRIGGER_CONDITION ((uint8) 0x03U) 231 #define WDG_API_GET_VERSION_INFO ((uint8) 0x04U) 233 #define WDG_API_TRIGGER ((uint8) 0x05U) 235 #define WDG_API_REGISTER_READBACK ((uint8) 0x06U) 245 #define WDG_WINDOW_100_PERCENT ((uint32) 0x00000005U) 247 #define WDG_WINDOW_50_PERCENT ((uint32) 0x00000050U) 249 #define WDG_WINDOW_25_PERCENT ((uint32) 0x00000500U) 251 #define WDG_WINDOW_12P5_PERCENT ((uint32) 0x00005000U) 253 #define WDG_WINDOW_6P25_PERCENT ((uint32) 0x00050000U) 255 #define WDG_WINDOW_3P125_PERCENT ((uint32) 0x00500000U) 259 #define INIT_VAL_ZERO (0U) 312 typedef struct Wdg_ConfigType_s
326 typedef struct Wdg_ConfigType_PC_s
335 #if (STD_ON == WDG_REGISTER_READBACK_API) 359 #if (STD_ON == WDG_GET_VERSION_INFO_API) 459 FUNC(Std_ReturnType, WDG_CODE)
Wdg_SetMode(WdgIf_ModeType Mode);
460 #if (STD_ON == WDG_REGISTER_READBACK_API) 489 WDG_APPL_DATA) regRbPtr);
uint32 windowSize
Definition: Wdg.h:301
uint32 rtiWdStatus
Definition: Wdg.h:342
Std_ReturnType Wdg_RegisterReadback(Wdg_RegisterReadbackType *regRbPtr)
This function reads the important registers of the hardware unit and returns the value in the structu...
void Wdg_SetTriggerCondition(uint16 timeout)
Sets the timeout value for the trigger counter.
WDG config structure.
Definition: Wdg.h:312
WDG pre-compile config structure.
Definition: Wdg.h:326
void Wdg_Init(const Wdg_ConfigType *CfgPtr)
This service initializes the WDG driver.
void Wdg_GetVersionInfo(Std_VersionInfoType *versioninfo)
This service returns the version information of this module.
uint32 reaction
Definition: Wdg.h:292
uint16 instanceId
Definition: Wdg.h:328
uint32 timeOutVal
Definition: Wdg.h:304
Std_ReturnType Wdg_SetMode(WdgIf_ModeType Mode)
This function triggers the servicing of the watchdog.
Mode info type.
Definition: Wdg.h:290
uint32 initialTimeOut
Definition: Wdg.h:330
uint32 rtiWwdSizeCtrl
Definition: Wdg.h:348
Wdg_ModeInfoType fastModeCfg
Definition: Wdg.h:316
WdgIf_ModeType defaultMode
Definition: Wdg.h:314
void Wdg_Trigger(void)
This function triggers the servicing of the watchdog.
uint32 rtiDwdprld
Definition: Wdg.h:340
This file contains generated pre compile configuration file for WDG MCAL driver.
Wdg_StatusType
Watchdog driver state.
Definition: Wdg.h:276
Wdg_ModeInfoType slowModeCfg
Definition: Wdg.h:318
uint32 rtiDwdCtrl
Definition: Wdg.h:338
uint32 rtiWdKey
Definition: Wdg.h:344
uint32 rtiWwdRxnCtrl
Definition: Wdg.h:346