108 #if (STD_ON == SPI_DMA_ENABLE) 115 #endif//#if (STD_ON == SPI_DMA_ENABLE) void Spi_IntISR_McuMcspiDmaRx(Spi_HWUnitType MaxHwUnit, Spi_HWUnitType Spi_HwUnit)
uint8 Spi_HWUnitType
Specifies the identification (ID) for a SPI Hardware micro controller peripheral (unit)
Definition: Spi.h:240
void Spi_IntISR_McuMcspiTxRx(Spi_HWUnitType Spi_HwUnit)
ADC ISR.
This file contains interface header for SPI MCAL driver.
void Spi_IntISR_McuMcspiDmaTx(Spi_HWUnitType MaxHwUnit, Spi_HWUnitType Spi_HwUnit)