![]() |
SDL API Guide for J7200
|
Slave TOG Static Registers.
This structure contains Slave TOG static registers The register values are not expected to change until a new configuration is done.
Data Fields | |
uint32_t | PID |
uint32_t | CFG |
uint32_t | ENABLE |
uint32_t | FLUSH |
uint32_t | TIMEOUT |
uint32_t | ERR |
uint32_t SDL_TOG_staticRegs::PID |
Revision Register
uint32_t SDL_TOG_staticRegs::CFG |
Configuration Register
uint32_t SDL_TOG_staticRegs::ENABLE |
Enable Register
uint32_t SDL_TOG_staticRegs::FLUSH |
Flush Register
uint32_t SDL_TOG_staticRegs::TIMEOUT |
Timeout Value Register
uint32_t SDL_TOG_staticRegs::ERR |
Error Interrupt Enabled Status/Set Register