![]() |
SDL API Guide for J7200
|
This structure contains the different configuration used for PBIST for the failure insertion test to generate negative result.
Design: PROC_SDL-977
Data Fields | |
uint32_t | CA0 |
uint32_t | CA1 |
uint32_t | CA2 |
uint32_t | CA3 |
uint32_t | CL0 |
uint32_t | CL1 |
uint32_t | CL2 |
uint32_t | CL3 |
uint32_t | CMS |
uint32_t | CSR |
uint32_t | I0 |
uint32_t | I1 |
uint32_t | I2 |
uint32_t | I3 |
uint32_t | RAMT |
uint32_t SDL_PBIST_configNeg::CA0 |
Failure insertion value for CA0 Value for the Failure Insertion Test Vector CA0
uint32_t SDL_PBIST_configNeg::CA1 |
Failure insertion value for CA1 Value for the Failure Insertion Test Vector CA1
uint32_t SDL_PBIST_configNeg::CA2 |
Failure insertion value for CA2 Value for the Failure Insertion Test Vector CA2
uint32_t SDL_PBIST_configNeg::CA3 |
Failure insertion value for CA3 Value for the Failure Insertion Test Vector CA3
uint32_t SDL_PBIST_configNeg::CL0 |
Failure insertion value for CL0 Value for the Failure Insertion Test Vector CL0
uint32_t SDL_PBIST_configNeg::CL1 |
Failure insertion value for CL1 Value for the Failure Insertion Test Vector CL1
uint32_t SDL_PBIST_configNeg::CL2 |
Failure insertion value for CL2 Value for the Failure Insertion Test Vector CL2
uint32_t SDL_PBIST_configNeg::CL3 |
Failure insertion value for CL3 Value for the Failure Insertion Test Vector CL3
uint32_t SDL_PBIST_configNeg::CMS |
Failure insertion value for CMS Value for the Failure Insertion Test Vector CMS
uint32_t SDL_PBIST_configNeg::CSR |
Failure insertion value for CSR Value for the Failure Insertion Test Vector CSR
uint32_t SDL_PBIST_configNeg::I0 |
Failure insertion value for I0 Value for the Failure Insertion Test Vector I0
uint32_t SDL_PBIST_configNeg::I1 |
Failure insertion value for I1 Value for the Failure Insertion Test Vector I1
uint32_t SDL_PBIST_configNeg::I2 |
Failure insertion value for I2 Value for the Failure Insertion Test Vector I2
uint32_t SDL_PBIST_configNeg::I3 |
Failure insertion value for I3 Value for the Failure Insertion Test Vector I3
uint32_t SDL_PBIST_configNeg::RAMT |
Failure insertion value for RAMT Value for the Failure Insertion Test Vector RAMT