![]() |
SDL API Guide for J7200
|
This structure defines the error status information.
Data Fields | |
SDL_ECC_MemType | eccMemType |
SDL_ECC_MemSubType | memSubType |
SDL_Ecc_AggrIntrSrc | intrSrc |
uint32_t | bitErrCnt |
uint32_t | injectBitErrCnt |
uint32_t | bitErrorGroup |
uint64_t | bitErrorOffset |
SDL_ECC_MemType SDL_ECC_ErrorInfo_t::eccMemType |
ECC Memory type
SDL_ECC_MemSubType SDL_ECC_ErrorInfo_t::memSubType |
Memory subtype
SDL_Ecc_AggrIntrSrc SDL_ECC_ErrorInfo_t::intrSrc |
Interrupt source
uint32_t SDL_ECC_ErrorInfo_t::bitErrCnt |
bit error count for the interrupt source. 0-2 Number of errors, 3 means 3 or more errors.
uint32_t SDL_ECC_ErrorInfo_t::injectBitErrCnt |
inject bit error count for the interrupt source (valid for EDC only). 0-2 Number of errors, 3 means 3 or more errors.
uint32_t SDL_ECC_ErrorInfo_t::bitErrorGroup |
bit error group. Indicates the Checker Group where the error occurred.
uint64_t SDL_ECC_ErrorInfo_t::bitErrorOffset |
bit error offset