![]() |
SDL API Guide for J7200
|
CCM Static Register.
This is the structure that is used to return the static registers in the static registers readback function
Data Fields | |
volatile uint32_t | CCMKEYR1 |
volatile uint32_t | CCMKEYR2 |
volatile uint32_t | CCMKEYR3 |
volatile uint32_t | CCMPOLCNTRL |
volatile uint32_t SDL_CCM_staticRegs::CCMKEYR1 |
volatile uint32_t SDL_CCM_staticRegs::CCMKEYR2 |
volatile uint32_t SDL_CCM_staticRegs::CCMKEYR3 |
volatile uint32_t SDL_CCM_staticRegs::CCMPOLCNTRL |