35 #ifndef SDL_VCL_SOC_TOG_H_ 36 #define SDL_VCL_SOC_TOG_H_ 39 #include <tistdtypes.h> 62 #define SDL_TOG_INSTANCE_MCU_INFRA0_CFG 0U 64 #define SDL_TOG_INSTANCE_MCU_FW1_CFG 1U 66 #define SDL_TOG_INSTANCE_MCU_64B2_CFG 2U 68 #define SDL_TOG_INSTANCE_WKUP_INFRA0_CFG 3U 70 #define SDL_TOG_INSTANCE_MCU_64B3_CFG 4U 72 #define SDL_TOG_INSTANCE_MCU_64B4_CFG 5U 74 #define SDL_TOG_INSTANCE_TIMEOUT0_CFG 6U 76 #define SDL_TOG_INSTANCE_TIMEOUT3_CFG 7U 78 #define SDL_TOG_INSTANCE_TIMEOUT4_CFG 8U 80 #define SDL_TOG_INSTANCE_TIMEOUT2_CFG 9U 82 #define SDL_TOG_INSTANCE_TIMEOUT1_CFG 10U 84 #define SDL_TOG_INSTANCE_PVU0_SRC 11U 86 #define SDL_TOG_INSTANCE_PVU0_CFG 12U 88 #define SDL_TOG_MAX_INSTANCE SDL_TOG_INSTANCE_PVU0_CFG 92 SDL_MCU_TIMEOUT_INFRA0_CFG_BASE,
93 SDL_MCU_TIMEOUT_FW1_CFG_BASE,
94 SDL_MCU_TIMEOUT_64B2_CFG_BASE,
95 SDL_WKUP_TIMEOUT_INFRA0_CFG_BASE,
96 SDL_MCU_TIMEOUT_64B3_CFG_BASE,
97 SDL_MCU_TIMEOUT_64B4_CFG_BASE,
98 SDL_TIMEOUT0_CFG_BASE,
99 SDL_TIMEOUT3_CFG_BASE,
100 SDL_TIMEOUT4_CFG_BASE,
101 SDL_TIMEOUT2_CFG_BASE,
102 SDL_TIMEOUT1_CFG_BASE,
103 SDL_NAVSS0_PVU0_SRC_TOG_CFG_BASE,
104 SDL_NAVSS0_PVU0_CFG_TOG_CFG_BASE
#define SDL_TOG_MAX_INSTANCE
Definition: sdl_soc_tog.h:88
uint8_t SDL_TOG_Inst
Definition: sdl_soc_tog.h:60
static uint32_t SDL_TOG_baseAddress[SDL_TOG_MAX_INSTANCE+1U]
Definition: sdl_soc_tog.h:90
This file contains SOC specific defintions.