![]() |
SDL API Guide for J7200
|
This file contains the SDL-FL API's for MSMC Scrubbing Engine.
This is the SDL-FL API documentation for the e Multicore Shared Memory Controller (MSMC) module.
Go to the source code of this file.
Macros | |
#define | SDL_MSMC_SCRUB_ENGINE_REGISTER (0x00003080UL) |
#define | SDL_MSMC_SCRUB_ENABLE_MASK (0x80000000UL) |
#define | SDL_MSMC_SCRUB_ENABLE_SHIFT (0x0000001FU) |
#define | SDL_MSMC_SCRUB_ENABLE_MAX (0x00000001UL) |
Functions | |
bool | SDL_MSMC_isScrubEnabled (void) |
Checks enable status of MSMC Scrubbing Engine. More... | |
#define SDL_MSMC_SCRUB_ENGINE_REGISTER (0x00003080UL) |
#define SDL_MSMC_SCRUB_ENABLE_MASK (0x80000000UL) |
#define SDL_MSMC_SCRUB_ENABLE_SHIFT (0x0000001FU) |
#define SDL_MSMC_SCRUB_ENABLE_MAX (0x00000001UL) |