![]() |
SDL API Guide for J7200
|
Go to the source code of this file.
Functions | |
int32_t | SDL_armR5ReadCCMRegister (uintptr_t baseAddress, SDL_McuArmssCcmR5RegId regId, uint32_t *pValToBeRead, int32_t *pMetaInfo) |
Read CCM Regiser. More... | |
int32_t | SDL_armR5ConfigureCCMRegister (uintptr_t baseAddress, SDL_McuArmssCcmR5RegId regId, uint32_t valToBeWritten, int32_t *pMetaInfo) |
Configure CCM Regiser. More... | |
int32_t | SDL_armR5CCMSetOperationModeKey (uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, SDL_McuArmssCcmR5OpModeKey opModeKey, int32_t *pMetaInfo) |
Configure Operating mode for CPU, VIM, CCM Inactivity monitor. More... | |
int32_t | SDL_armR5CCMGetCompareError (uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, uint32_t *pCmpError, int32_t *pMetaInfo) |
Read Compare Error status for CPU, VIM, CCM Inactivity monitor. More... | |
int32_t | SDL_armR5CCMGetOperationModeKey (uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, SDL_McuArmssCcmR5OpModeKey *pOpModeKey, int32_t *pMetaInfo) |
Get Operation mode key value for CPU, VIM, CCM Inactivity monitor. More... | |
int32_t | SDL_armR5CCMClearCompareError (uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, int32_t *pMetaInfo) |
Clear Compare Error value for CPU, VIM, CCM Inactivity monitor. More... | |