SDL API Guide for J7200
sdl/sdl_esm.h
Go to the documentation of this file.
1 /********************************************************************
2  * Copyright (C) 2021 Texas Instruments Incorporated.
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  *
32  */
33 
44 #ifndef SDL_ESM_H_
45 #define SDL_ESM_H_
46 
47 #ifdef __cplusplus
48 extern "C" {
49 #endif
50 
51 #include <src/ip/sdl_ip_esm.h>
52 
87 int32_t SDL_ESM_getNErrorStatus(SDL_ESM_Inst instance, uint32_t *pStatus);
88 
103 int32_t SDL_ESM_getStaticRegisters(SDL_ESM_Inst instance, SDL_ESM_staticRegs *pStaticRegs);
104 
118 int32_t SDL_ESM_verifyConfig(SDL_ESM_Inst instance, const SDL_ESM_config *pConfig);
119 
129 int32_t SDL_ESM_clrNError(SDL_ESM_Inst instance);
130 
140 int32_t SDL_ESM_setNError(SDL_ESM_Inst instance);
141 
163 int32_t SDL_ESM_registerECCCallback(SDL_ESM_Inst instance, uint32_t eventBitMap[],
164  SDL_ESM_applicationCallback eccCallback,
165  void *callbackArg);
166 
189 int32_t SDL_ESM_registerCCMCallback(SDL_ESM_Inst instance, uint32_t eventBitMap[],
190  SDL_ESM_applicationCallback ccmCallback,
191  void *callbackArg);
192 
213 int32_t SDL_ESM_init(SDL_ESM_Inst instance, const SDL_ESM_config *pConfig,
214  SDL_ESM_applicationCallback applicationCallback, void *appArg);
215 
218 #ifdef __cplusplus
219 }
220 #endif
221 
222 #endif /* SDL_ESM_H_ */
ESM static registers list.
Definition: esm.h:237
SDL_ESM_Inst
Defines the different ESM instance types
Definition: ip/sdl_esm.h:167
int32_t SDL_ESM_registerECCCallback(SDL_ESM_Inst instance, uint32_t eventBitMap[], SDL_ESM_applicationCallback eccCallback, void *callbackArg)
There are modules within SDL which will generate ESM errors intentionally in the course of running se...
int32_t SDL_ESM_verifyConfig(SDL_ESM_Inst instance, const SDL_ESM_config *pConfig)
SDL ESM API to verify the written configuration of the ESM module. The API verifies the written confi...
int32_t SDL_ESM_clrNError(SDL_ESM_Inst instance)
SDL ESM API to clear the nError pin for the specified ESM instance.
ESM init configuration.
Definition: ip/sdl_esm.h:285
int32_t SDL_ESM_getNErrorStatus(SDL_ESM_Inst instance, uint32_t *pStatus)
SDL ESM API to get the status of the nError pin for the specified ESM instance.
int32_t SDL_ESM_init(SDL_ESM_Inst instance, const SDL_ESM_config *pConfig, SDL_ESM_applicationCallback applicationCallback, void *appArg)
SDL ESM API to initialize an ESM instance. The API initializes the specified ESM instance with the pr...
int32_t(* SDL_ESM_applicationCallback)(SDL_ESM_Inst instance, SDL_ESM_IntType intrType, uint32_t grpChannel, uint32_t index, uint32_t intSrc, void *arg)
Definition: ip/sdl_esm.h:263
int32_t SDL_ESM_setNError(SDL_ESM_Inst instance)
SDL ESM API to set the nError pin for the specified ESM instance.
int32_t SDL_ESM_registerCCMCallback(SDL_ESM_Inst instance, uint32_t eventBitMap[], SDL_ESM_applicationCallback ccmCallback, void *callbackArg)
There are modules within SDL which will generate ESM errors intentionally in the course of running se...
int32_t SDL_ESM_getStaticRegisters(SDL_ESM_Inst instance, SDL_ESM_staticRegs *pStaticRegs)
SDL ESM API to read the static registers. The API reads and returns the static register configuration...