![]() |
SDL API Guide for J7200
|
===========================================================================
Timeout interrupt sources | |
This enumerator defines the possible timeout interrupt sources | |
typedef uint32_t | SDL_TOG_IntrSrc |
#define | SDL_TOG_INTRSRC_TRANSACTION_TIMEOUT ((uint32_t) 1U<<0) |
#define | SDL_TOG_INTRSRC_UNEXPECTED_RESPONSE ((uint32_t) 1U<<1) |
#define | SDL_TOG_INTRSRC_COMMAND_TIMEOUT ((uint32_t) 1U<<2) |
#define | SDL_TOG_INTRSRC_ALL (SDL_TOG_INTRSRC_TRANSACTION_TIMEOUT | SDL_TOG_INTRSRC_UNEXPECTED_RESPONSE | SDL_TOG_INTRSRC_COMMAND_TIMEOUT) |
#define SDL_TOG_INTRSRC_TRANSACTION_TIMEOUT ((uint32_t) 1U<<0) |
Transaction timeout
#define SDL_TOG_INTRSRC_UNEXPECTED_RESPONSE ((uint32_t) 1U<<1) |
Unexpected response
#define SDL_TOG_INTRSRC_COMMAND_TIMEOUT ((uint32_t) 1U<<2) |
Command timeout
#define SDL_TOG_INTRSRC_ALL (SDL_TOG_INTRSRC_TRANSACTION_TIMEOUT | SDL_TOG_INTRSRC_UNEXPECTED_RESPONSE | SDL_TOG_INTRSRC_COMMAND_TIMEOUT) |
All interrupt sources
typedef uint32_t SDL_TOG_IntrSrc |