SDL API Guide for J7200
|
Functions | |
int32_t | SDL_OSAL_init (SDL_OSAL_Interface *osalInterface) |
OSAL init. More... | |
int32_t | SDL_OSAL_enableInterrupt (int32_t intNum) |
OSAL enable interrupt. More... | |
int32_t | SDL_OSAL_disableInterrupt (int32_t intNum) |
OSAL disable interrupt. More... | |
int32_t | SDL_OSAL_registerInterrupt (SDL_OSAL_hwipParams *pParams, pSDL_OSAL_hwipHandle *handle) |
OSAL register interrupt. More... | |
int32_t | SDL_OSAL_deregisterInterrupt (pSDL_OSAL_hwipHandle handle) |
OSAL deregister interrupt. More... | |
int32_t | SDL_OSAL_globalDisableInterrupts (uintptr_t *key) |
OSAL globally disable interrupts. More... | |
int32_t | SDL_OSAL_globalRestoreInterrupts (uintptr_t key) |
OSAL globally enable interrupts. More... | |
void | SDL_OSAL_printf (const char *traceBuf) |
OSAL print function. More... | |
int32_t | SDL_OSAL_delay (int32_t ndelay) |
OSAL delay. More... | |
void * | SDL_OSAL_addrTranslate (uint64_t addr, uint32_t size) |
OSAL Address translation function. More... | |
int32_t SDL_OSAL_init | ( | SDL_OSAL_Interface * | osalInterface | ) |
OSAL init.
This function initializes the OSAL interface structure with the functions provided by the application. These functions are application dependent, so it is required to be passed by the user.
osalInterface | [IN] OSAL interface structure. |
int32_t SDL_OSAL_enableInterrupt | ( | int32_t | intNum | ) |
OSAL enable interrupt.
This function will enable the specific interrupt number passed.
intNum | [IN] Interrupt Number |
int32_t SDL_OSAL_disableInterrupt | ( | int32_t | intNum | ) |
OSAL disable interrupt.
This function will disable the specific interrupt number passed.
intNum | [IN] Interrupt Number |
int32_t SDL_OSAL_registerInterrupt | ( | SDL_OSAL_hwipParams * | pParams, |
pSDL_OSAL_hwipHandle * | handle | ||
) |
OSAL register interrupt.
This function will register the specific interrupt number passed.
pParams | [IN] Parameters for interrupt registration |
handle | [OUT] Handle for this registered interrupt |
int32_t SDL_OSAL_deregisterInterrupt | ( | pSDL_OSAL_hwipHandle | handle | ) |
OSAL deregister interrupt.
This function will deregister the specific interrupt number passed.
handle | [IN] Handle for the registered interrupt |
int32_t SDL_OSAL_globalDisableInterrupts | ( | uintptr_t * | key | ) |
OSAL globally disable interrupts.
This function will disable interrupts globally. Interrupts can be enabled with the globalRestoreInterrupts() function. Usually used for critical sections.
The returned key is used to restore the context once interrupts are restored.
key | [OUT] key to use when restoring interrupts |
int32_t SDL_OSAL_globalRestoreInterrupts | ( | uintptr_t | key | ) |
OSAL globally enable interrupts.
This function will enable interrupts globally. Usually used for critical sections.
The key is used to restore the context.
key | [IN] key to use when restoring interrupts |
void SDL_OSAL_printf | ( | const char * | traceBuf | ) |
OSAL print function.
This function prints the provided string
traceBuf | [IN] String to be printed |
int32_t SDL_OSAL_delay | ( | int32_t | ndelay | ) |
OSAL delay.
This function is used assign delay in the function
ndelay | [IN] delay in microseconds |
void* SDL_OSAL_addrTranslate | ( | uint64_t | addr, |
uint32_t | size | ||
) |
OSAL Address translation function.
This function is used by the SDL to get a translation for a 64-bit address to local address space. It is expected that the requested adddress will remain available at the returned address and not be removed.
addr | [IN] Memory address to be translated |
size | [IN] Size of the memory |