![]() |
SDL API Guide for J7200
|
Functions | |
void | SDL_VTM_getSensorVDCount (const SDL_VTM_cfg1Regs *p_cfg1) |
get sensor and VD count More... | |
SDL_VTM_adc_code | SDL_VTM_getBestValue (SDL_VTM_adc_code c0, SDL_VTM_adc_code c1, SDL_VTM_adc_code c2) |
select best ADC code More... | |
SDL_VTM_adc_code | SDL_VTM_getAdcCode (const SDL_VTM_cfg1Regs_TMPSENS *p_sensor) |
read Temperature sensor ADC code More... | |
int32_t | SDL_VTM_vdSetOppVid (const SDL_VTM_cfg1Regs *p_cfg1, SDL_VTM_InstVd instance, SDL_VTM_vid_opp vid_opp, uint8_t vid_opp_val) |
set the VID OPP Code for VID OPP register More... | |
int32_t | SDL_VTM_vdGetOppVid (const SDL_VTM_cfg1Regs *p_cfg1, SDL_VTM_InstVd instance, SDL_VTM_vid_opp vid_opp, uint8_t *p_vid_opp_val) |
get VTM VID OPP Code from VID OPP register More... | |
int32_t | SDL_VTM_vdEvtSelSet (const SDL_VTM_cfg1Regs *p_cfg1, SDL_VTM_InstVd instance, SDL_VTM_vdEvtSel_set vd_temp_evts) |
set Voltage domain a event select and control set register. In this API, select which of the event contributions of the temp-monitors controlled by this VTM will contribute to generate the merged event/alerts of this VD. Any combination of them could be selected More... | |
int32_t | SDL_VTM_tsSetGlobalCfg (const SDL_VTM_cfg2Regs *p_cfg2, const SDL_VTM_tsGlobal_cfg *p_tsGlobal_cfg) |
VTM Temperature Sensor Set Global configuration values. More... | |
int32_t | SDL_VTM_tsGetGlobalCfg (const SDL_VTM_cfg2Regs *p_cfg2, SDL_VTM_tsGlobal_cfg *p_tsGlobal_cfg) |
VTM Temperature Sensor Get Global configuration values. More... | |
int32_t | SDL_VTM_tsSetCtrl (const SDL_VTM_cfg2Regs *p_cfg2, SDL_VTM_InstTs instance, const SDL_VTM_Ctrlcfg *p_tsCtrl_cfg) |
VTM Temperature Sensor Control. More... | |
int32_t | SDL_VTM_tsGetCtrl (const SDL_VTM_cfg2Regs *p_cfg2, SDL_VTM_InstTs instance, SDL_VTM_Ctrlcfg *p_tsCtrl_cfg) |
Read VTM Temperature Sensor Control. More... | |
int32_t | SDL_VTM_tsSetThresholds (const SDL_VTM_cfg1Regs *p_cfg1, SDL_VTM_InstTs instance, const SDL_VTM_tsThrVal *p_thr_val) |
VTM Temperature sensor set, clear threshold values and enable, disable threshold events. More... | |
int32_t | SDL_VTM_tsGetThresholds (const SDL_VTM_cfg1Regs *p_cfg1, SDL_VTM_InstTs instance, SDL_VTM_tsThrVal *p_thr_val) |
VTM Temperature Sensor get threshold values and threshold enable/disable status. More... | |
int32_t | SDL_VTM_tsConvADCToTemp (SDL_VTM_adc_code adc_code, SDL_VTM_InstTs instance, int32_t *p_milli_degree_temp_val) |
VTM Temperature ADC code to Temperature conversion. More... | |
int32_t | SDL_VTM_tsConvTempToAdc (int32_t milli_degree_temp_val, SDL_VTM_InstTs instance, SDL_VTM_adc_code *p_adc_code) |
VTM Temperature to ADC code conversion. More... | |
int32_t | SDL_VTM_tsSetMaxTOutRgAlertThr (const SDL_VTM_cfg2Regs *p_cfg2, SDL_VTM_InstTs instance, int32_t high_temp_in_milli_degree_celcius, int32_t low_temp_in_milli_degree_celcius) |
VTM Temperature Sensor Maximum Temperature Out of Range Alert threshold. More... | |
void SDL_VTM_getSensorVDCount | ( | const SDL_VTM_cfg1Regs * | p_cfg1 | ) |
get sensor and VD count
p_cfg1 | [IN] Pointer to the VTM configuration1 structure |
SDL_VTM_adc_code SDL_VTM_getBestValue | ( | SDL_VTM_adc_code | c0, |
SDL_VTM_adc_code | c1, | ||
SDL_VTM_adc_code | c2 | ||
) |
select best ADC code
c0 | [IN] ADC code 0 |
c1 | [IN] ADC code 1 |
c2 | [IN] ADC code 2 |
SDL_VTM_adc_code SDL_VTM_getAdcCode | ( | const SDL_VTM_cfg1Regs_TMPSENS * | p_sensor | ) |
read Temperature sensor ADC code
p_sensor | [IN] Pointer to the sensor code |
int32_t SDL_VTM_vdSetOppVid | ( | const SDL_VTM_cfg1Regs * | p_cfg1, |
SDL_VTM_InstVd | instance, | ||
SDL_VTM_vid_opp | vid_opp, | ||
uint8_t | vid_opp_val | ||
) |
set the VID OPP Code for VID OPP register
Reset defaults are sourced from efuse for each OPP. The default reset values will not be necessarily overwritten. The write capability in the MMR is for having the option to debug and have software driven adjustments if necessary
p_cfg1 | [IN] Pointer to the VTM configuration1 structure |
instance | [IN] VTM Voltage Domain instance |
vid_opp | [IN] which VID OPP to be updated |
vid_opp_val | [IN] VID OPP Code value |
int32_t SDL_VTM_vdGetOppVid | ( | const SDL_VTM_cfg1Regs * | p_cfg1, |
SDL_VTM_InstVd | instance, | ||
SDL_VTM_vid_opp | vid_opp, | ||
uint8_t * | p_vid_opp_val | ||
) |
get VTM VID OPP Code from VID OPP register
p_cfg1 | [IN] Pointer to the VTM configuration1 structure |
instance | [IN] VTM Voltage Domain instance |
vid_opp | [IN] which VID OPP to be updated |
p_vid_opp_val | [OUT] Pointer to VID OPP Code value |
int32_t SDL_VTM_vdEvtSelSet | ( | const SDL_VTM_cfg1Regs * | p_cfg1, |
SDL_VTM_InstVd | instance, | ||
SDL_VTM_vdEvtSel_set | vd_temp_evts | ||
) |
set Voltage domain a event select and control set register. In this API, select which of the event contributions of the temp-monitors controlled by this VTM will contribute to generate the merged event/alerts of this VD. Any combination of them could be selected
p_cfg1 | [IN] Pointer to the VTM configuration1 structure |
instance | [IN] VTM Voltage Domain instance |
vd_temp_evts | [IN] Temperature events to be selected for VD |
int32_t SDL_VTM_tsSetGlobalCfg | ( | const SDL_VTM_cfg2Regs * | p_cfg2, |
const SDL_VTM_tsGlobal_cfg * | p_tsGlobal_cfg | ||
) |
VTM Temperature Sensor Set Global configuration values.
p_cfg2 | [IN] Pointer to the VTM configuration2 structure |
p_tsGlobal_cfg | [IN] Pointer to temperature global configuration |
int32_t SDL_VTM_tsGetGlobalCfg | ( | const SDL_VTM_cfg2Regs * | p_cfg2, |
SDL_VTM_tsGlobal_cfg * | p_tsGlobal_cfg | ||
) |
VTM Temperature Sensor Get Global configuration values.
p_cfg2 | [IN] Pointer to the VTM configuration2 structure |
p_tsGlobal_cfg | [OUT] Pointer to temperature global configuration |
int32_t SDL_VTM_tsSetCtrl | ( | const SDL_VTM_cfg2Regs * | p_cfg2, |
SDL_VTM_InstTs | instance, | ||
const SDL_VTM_Ctrlcfg * | p_tsCtrl_cfg | ||
) |
VTM Temperature Sensor Control.
p_cfg2 | [IN] Pointer to the VTM configuration2 structure |
instance | [IN] VTM Temperature sensor instance |
p_tsCtrl_cfg | [IN] Pointer to temperature sensor control configuration |
int32_t SDL_VTM_tsGetCtrl | ( | const SDL_VTM_cfg2Regs * | p_cfg2, |
SDL_VTM_InstTs | instance, | ||
SDL_VTM_Ctrlcfg * | p_tsCtrl_cfg | ||
) |
Read VTM Temperature Sensor Control.
p_cfg2 | [IN] Pointer to the VTM configuration2 structure |
instance | [IN] VTM Temperature sensor instance |
p_tsCtrl_cfg | [IN] Pointer to temperature sensor control configuration |
int32_t SDL_VTM_tsSetThresholds | ( | const SDL_VTM_cfg1Regs * | p_cfg1, |
SDL_VTM_InstTs | instance, | ||
const SDL_VTM_tsThrVal * | p_thr_val | ||
) |
VTM Temperature sensor set, clear threshold values and enable, disable threshold events.
p_cfg1 | [IN] Pointer to the VTM configuration1 structure |
instance | [IN] VTM Temperature sensor instance |
p_thr_val | [IN] Pointer to temperature threshold values |
int32_t SDL_VTM_tsGetThresholds | ( | const SDL_VTM_cfg1Regs * | p_cfg1, |
SDL_VTM_InstTs | instance, | ||
SDL_VTM_tsThrVal * | p_thr_val | ||
) |
VTM Temperature Sensor get threshold values and threshold enable/disable status.
p_cfg1 | [IN] Pointer to the VTM configuration1 structure |
instance | [IN] VTM Temperature sensor instance |
p_thr_val | [OUT] Pointer to temperature threshold values |
int32_t SDL_VTM_tsConvADCToTemp | ( | SDL_VTM_adc_code | adc_code, |
SDL_VTM_InstTs | instance, | ||
int32_t * | p_milli_degree_temp_val | ||
) |
VTM Temperature ADC code to Temperature conversion.
adc_code | [IN] 10 Bit ADC code |
instance | [IN] VTM Temperature sensor instance |
p_milli_degree_temp_val | [OUT] Pointer to Temperature in milli degree celcius |
int32_t SDL_VTM_tsConvTempToAdc | ( | int32_t | milli_degree_temp_val, |
SDL_VTM_InstTs | instance, | ||
SDL_VTM_adc_code * | p_adc_code | ||
) |
VTM Temperature to ADC code conversion.
milli_degree_temp_val | [IN] Temperature in milli degree celcius |
instance | [IN] VTM Temperature sensor instance |
p_adc_code | [OUT] Pointer to 10 Bit ADC code |
int32_t SDL_VTM_tsSetMaxTOutRgAlertThr | ( | const SDL_VTM_cfg2Regs * | p_cfg2, |
SDL_VTM_InstTs | instance, | ||
int32_t | high_temp_in_milli_degree_celcius, | ||
int32_t | low_temp_in_milli_degree_celcius | ||
) |
VTM Temperature Sensor Maximum Temperature Out of Range Alert threshold.
This function sets the "high temperature threshold" and "low temperature threshold" alert thresholds for the VTM hardware to use in determining when to apply the device reset (and when to release it). When the temperatures are above the high threshold, a SoC reset would be done and gets released after the temperature falls below the low temperature threshold. There should not be any ISR (Interrupt Service Routine) need to program for maximum temperature out of range programming. The caller should have actively taken necessary cooling actions, prior to temperature reaching to this maximum value, with the help of GT_THR1 and/or GT_THR2 alert ISRs.
p_cfg2 | [IN] Pointer to the VTM configuration2 structure |
instance | [IN] VTM Temperature sensor instance |
high_temp_in_milli_degree_celcius | [IN] high temperature in milli degree celcius |
low_temp_in_milli_degree_celcius | [IN] low temperature in milli degree celcius |