![]() |
SDL API Guide for J7200
|
Typedefs | |
typedef void(* | SDL_EXCEPTION_ECCCallback_t) (uint32_t intSource, uint32_t errorAddr, uint32_t ramId, uint64_t bitErrorOffset, uint32_t bitErrorGroup) |
Format of Call back function for ECC error events. More... | |
typedef void(* | SDL_EXCEPTION_Callback_t) (void) |
Format of Call back function for exception. More... | |
typedef void(* SDL_EXCEPTION_ECCCallback_t) (uint32_t intSource, uint32_t errorAddr, uint32_t ramId, uint64_t bitErrorOffset, uint32_t bitErrorGroup) |
Format of Call back function for ECC error events.
typedef void(* SDL_EXCEPTION_Callback_t) (void) |
Format of Call back function for exception.