3.1. ESM Safety Example

3.1.1. Introduction

This example demonstrates High and Low priority events received from the WKUP_ESM, MCU_ESM, and ESM (Main domain ESM) through the application-registered callback. It also shows routing and clearing of events to the MCU_SAFETY_ERRORn pin.

This example displays setting up ESM to

  • Enable/Disable input events to the ESM module for each ESM instance

  • Registration of application callback for ESM error events for each ESM instance

  • Designating input events as high priority or low priority for each ESM instance

  • Designating direct pin routing to MCU_SAFETY_ERRORn pin for external monitor communication

The following modules are used as triggers to monitor and handle ESM events:

  • Voltage and Thermal Manager (VTM)

  • Timer

  • ECC

3.1.2. Use Cases

Use Case

Description

ESM

Input Event

Input Trigger

Priority

Action

UC-1

Configuration of Low Priority ESM event with no error pin trigger using WKUP_ESM0. Error event is triggered and app is notified of event

WKUP_ESM0

WKUP_VTM0_THERM_LVL_GT_TH1_INTR_0 Temp greature than early warning threshold

Change threshold in VTM to trigger early warning, then return thresholds back to normal to simulate “cooling down”.

Low

Error event is logged by application. Print event to UART. Error event is cleared

UC-2

Configuration of High Priority ESM event with error pin trigger using WKUP_ESM0. Application handles the error event in software and clears the error pin.

WKUP_ESM0

WKUP_VTM0_THERM_LVL_GT_TH2_INTR_0

Change threshold in VTM to trigger early warning, then alter thresholds again to pass temperature critical threshold. Lastly, return thresholds back to normal to simulate “cooling down”.

High

Error event is logged by application. Print event to UART. Application clears error pin to simulate resolution of event by software.

UC-3

Configuration of High Priority ESM event with error pin trigger. Applicatino is unable to handle the error event in software and does not clear the error pin.

WKUP_ESM0

WKUP_VTM0_THERM_LVL_GT_TH2_INTR_0

Change threshold i nVTM to trigger early warning, then alter thresholds again to pass temperature critical threshold. Lastly, return thresholds back to normal to simulate “cooling down”.

High

Error event is logged by application. Print event to UART. Application does not clear the error pin in order to simulate no internal resolution by software. Simulates notification to external monitor.

UC-4

Configuration of Low Priority ESM event with no error pin trigger using MCU_ESM0. Error is triggered and application is notified of the event.

MCU_ESM0

MCU_TIMER3_INTR_PEND_0

Timer expiration

Low

Error event is logged by application. Print event to UART. Error event is cleared and execution continues.

UC-5

Configuration of High Priority ESM event with error pin trigger using MCU_ESM0. Application handles the error event in software and clears the error pin.

MCU_ESM0

MCU_TIMER2_INTR_PEND_0

Timer expiration

High

Error event is logged by application. Print event to UART. Application clears error pin to simulate resolution of event by software.

UC-6

Configuration of Low Priority ESM event with no error pin trigger using ESM0. Error event is triggered and app is notified of event.

ESM0

ECC error injection

Low

Error event is logged by application. Print event to UART. Error event is cleared and execution continues.

UC-7

Configuration of Hishg Priority ESM event with error pin trigger using ESM0. Application handles the error event in software and clears the error pin.

ESM0

ECC error injection

High

Error event is logged by application. Print event to UART. Application clears error pin to simulate resolution of event by software.

3.1.3. Example Details

The example should be loaded to the hardware using the Secondary Boot Loader (SBL) from the SDK.

Example Name

Location

Build Command

esm_wkup_mcu_app

[sdl_install_dir]/examples/esm/wkup_mcu_esm0/

make esm_wkup_mcu_app PROFILE=release

esm_main_app

[sdl_install_dir]/examples/esm/main_esm0/

make esm_main_app PROFILE=release

3.1.4. Expected Output

esm_wkup_mcu_app:

ESM Example Application

VTM_ESM_init: Init WKUP ESM complete

TIMER_ESM_init: Init MCU ESM complete

ESM example init complete
  Any clear of MCU_SAFETY_ERRORn pin will first wait 10 usecs
  Minimum Time Interval is 99 usecs
ESM timer initialization complete

Starting Test Case 0

  ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x8, intSrc 0x8
  Take action
  ESM instance #1, ESM interrupt type = Low Priority ESM event

    Got ltThr0 interrupt through ESM module

    System at a temperature below the threshold of lt_thr0
    System running at a safe temperature

  ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x9, intSrc 0x9
  Take action
  ESM instance #1, ESM interrupt type = Low Priority ESM event

  ESM Call back function called : instType 0x1, intType 0x1, grpChannel 0x0, index 0xa, intSrc 0xa
  Take action
  ESM instance #1, ESM interrupt type = High Priority ESM event
case 0 sucess

Use Case 0 completed: Input Event Trigger = Step completed successfully,
                       Event Handler Complete = Step completed successfully,
                       MCU_SAFETY_ERRORn Pin Clear = Step completed successfully

Starting Test Case 1

  ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x8, intSrc 0x8
  Take action
  ESM instance #1, ESM interrupt type = Low Priority ESM event

  ESM Call back function called : instType 0x1, intType 0x1, grpChannel 0x0, index 0xa, intSrc 0xa
  Take action
  ESM instance #1, ESM interrupt type = High Priority ESM event

  ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x8, intSrc 0x8
  Take action
  ESM instance #1, ESM interrupt type = Low Priority ESM event

    Got ltThr0 interrupt through ESM module

    System at a temperature below the threshold of lt_thr0
    System running at a safe temperature

  ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x9, intSrc 0x9
  Take action
  ESM instance #1, ESM interrupt type = Low Priority ESM event

  timerExpPinDisable: before clear, ESM instance 1 view of MCU_SAFETY_ERRORn pin is 0
case 1 sucess

Use Case 1 completed: Input Event Trigger = Step completed successfully,
                       Event Handler Complete = Step completed successfully,
                       MCU_SAFETY_ERRORn Pin Clear = Step completed successfully

Starting Test Case 2

  ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x8, intSrc 0x8
  Take action
  ESM instance #1, ESM interrupt type = Low Priority ESM event

  ESM Call back function called : instType 0x1, intType 0x1, grpChannel 0x0, index 0xa, intSrc 0xa
  Take action
  ESM instance #1, ESM interrupt type = High Priority ESM event

  timerExpPinDisable: before clear, ESM instance 1 view of MCU_SAFETY_ERRORn pin is 0

  ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x8, intSrc 0x8
  Take action
  ESM instance #1, ESM interrupt type = Low Priority ESM event

    Got ltThr0 interrupt through ESM module

    System at a temperature below the threshold of lt_thr0
    System running at a safe temperature

  ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x9, intSrc 0x9
  Take action
  ESM instance #1, ESM interrupt type = Low Priority ESM event

Use Case 2 completed: Input Event Trigger = Step completed successfully,
                       Event Handler Complete = Step completed successfully,
                       MCU_SAFETY_ERRORn Pin Clear = Step completed successfully

Starting Test Case 3
ERR: Unexpected ESM Instance 2 and ESM Interrupt Type 2

  ESM Call back function called : instType 0x2, intType 0x2, grpChannel 0x1, index 0x19, intSrc 0x39
  Take action
  ESM instance #2, ESM interrupt type = Low Priority ESM event

Use Case 3 completed: Input Event Trigger = Step completed successfully,
                       Event Handler Complete = Step completed successfully,
                       MCU_SAFETY_ERRORn Pin Clear = Step completed successfully

Starting Test Case 4
ERR: Unexpected ESM Instance 2 and ESM Interrupt Type 1

  ESM Call back function called : instType 0x2, intType 0x1, grpChannel 0x1, index 0x18, intSrc 0x38
  Take action
  ESM instance #2, ESM interrupt type = High Priority ESM event

  timerExpPinDisable: before clear, ESM instance 2 view of MCU_SAFETY_ERRORn pin is 0

Use Case 4 completed: Input Event Trigger = Step completed successfully,
                       Event Handler Complete = Step completed successfully,
                       MCU_SAFETY_ERRORn Pin Clear = Step completed successfully


ESM Example Application summary
-------------------------------
Completed 5 Test Cases
Received 4 High Priority Interrupts
Received 9 Low Priority Interrupts

Test Case Event Log
------------------

Test Case 0: ESM Call back function called : grpChannel 0x0, index 0x8, intSrc 0x8
  ESM instance #1, ESM interrupt type = Low Priority ESM event

Test Case 0: ESM Call back function called : grpChannel 0x0, index 0x9, intSrc 0x9
  ESM instance #1, ESM interrupt type = Low Priority ESM event

Test Case 0: ESM Call back function called : grpChannel 0x0, index 0xa, intSrc 0xa
  ESM instance #1, ESM interrupt type = High Priority ESM event

Test Case 1: ESM Call back function called : grpChannel 0x0, index 0x8, intSrc 0x8
  ESM instance #1, ESM interrupt type = Low Priority ESM event

Test Case 1: ESM Call back function called : grpChannel 0x0, index 0xa, intSrc 0xa
  ESM instance #1, ESM interrupt type = High Priority ESM event

Test Case 1: ESM Call back function called : grpChannel 0x0, index 0x8, intSrc 0x8
  ESM instance #1, ESM interrupt type = Low Priority ESM event

Test Case 1: ESM Call back function called : grpChannel 0x0, index 0x9, intSrc 0x9
  ESM instance #1, ESM interrupt type = Low Priority ESM event

Test Case 2: ESM Call back function called : grpChannel 0x0, index 0x8, intSrc 0x8
  ESM instance #1, ESM interrupt type = Low Priority ESM event

Test Case 2: ESM Call back function called : grpChannel 0x0, index 0xa, intSrc 0xa
  ESM instance #1, ESM interrupt type = High Priority ESM event

Test Case 2: ESM Call back function called : grpChannel 0x0, index 0x8, intSrc 0x8
  ESM instance #1, ESM interrupt type = Low Priority ESM event

Test Case 2: ESM Call back function called : grpChannel 0x0, index 0x9, intSrc 0x9
  ESM instance #1, ESM interrupt type = Low Priority ESM event

Test Case 3: ESM Call back function called : grpChannel 0x1, index 0x19, intSrc 0x39
  ESM instance #2, ESM interrupt type = Low Priority ESM event

Test Case 4: ESM Call back function called : grpChannel 0x1, index 0x18, intSrc 0x38
  ESM instance #2, ESM interrupt type = High Priority ESM event

ESM Example Application: Complete
 All Use cases have passed.
esm_input_trig.c:638:esm_app:PASS

-----------------------
1 Tests 0 Failures 0 Ignored

esm_main_app:

ESM Example Application

ESM_ECC_Example_init: Init MAIN ESM complete

SDTF_init: MCU MSMC ECC Init complete

ESM_ECC_Example_init: ECC Callback Init complete for Main ESM

 ESM Safety Example tests: starting
 MSMC Double bit error inject Example test UC-6: starting
  ESM Call back function called : instType 0x3, intType 0x2, grpChannel 0x1, index 0x10, intSrc 0x30
  Take action
 Low Priority Interrupt Executed

  ECC Error Call back function called : eccMemType 16, errorSrc 0x2, ramId 107, bitErrorOffset 0x00000000, bitErrorGroup 0

 MSMC Double bit error inject test: Subtype 0x6b test complete
 UC-6: Got Low priority ESM Interrupt

 MSMC Double bit error inject Example test UC-7: starting
  ESM Call back function called : instType 0x3, intType 0x1, grpChannel 0x1, index 0x11, intSrc 0x31
  Take action
 High Priority Interrupt Executed

  ECC Error Call back function called : eccMemType 16, errorSrc 0x1, ramId 20, bitErrorOffset 0x00000000, bitErrorGroup 0

 MSMC Double bit error inject test: Subtype 0x14 test complete
 UC-7: Got High priority ESM Interrupt

 ESM Safety Example tests: success
 ESM UC-6 and UC-7 Test Passed.

All Use_Cases have passed.
main.c:292:esm_app:PASS

-----------------------
1 Tests 0 Failures 0 Ignored

3.1.5. Reference

ESM User Guide