PDK API Guide for J7200
|
Input args for CPSW_ALE_IOCTL_SET_POLICER_THREADCFG command.
Configuration to set the thread/flow id associated with a classifier.
Data Fields | |
CpswAle_PolicerMatchParams | policerMatch |
bool | threadIdEn |
uint32_t | threadId |
CpswAle_PolicerMatchParams CpswAle_SetPolicerThreadCfgInArgs::policerMatch |
Policer match config
bool CpswAle_SetPolicerThreadCfgInArgs::threadIdEn |
Enable/disable thread id setting for this policer entry
uint32_t CpswAle_SetPolicerThreadCfgInArgs::threadId |
Thread Id which will be enabled for this policer match