PDK API Guide for J7200
|
MuxIntcP interface
Files | |
file | MuxIntcP.h |
Interrupt Controller Mux module for the RTOS Porting Interface. | |
Data Structures | |
struct | MuxIntcP_inParams |
Basic MuxIntcP Input Parameters. More... | |
struct | MuxIntcP_outParams |
Basic MuxIntcP Output Parameters. More... | |
Functions | |
MuxIntcP_Status | MuxIntcP_create (MuxIntcP_inParams *inParams, MuxIntcP_outParams *outParams) |
Function to create an interrupt controller mux. More... | |
void | MuxIntcP_enableInEvent (int32_t muxNum, int32_t muxInEvent) |
Function to enable interrupt controller mux for an input event. More... | |
void | MuxIntcP_disableInEvent (int32_t muxNum, int32_t muxInEvent) |
Function to disable interrupt controller mux for an input event. More... | |
void | MuxIntcP_clearInEvent (int32_t muxNum, int32_t muxInEvent) |
Function to clear interrupt controller mux for an input event. More... | |
void | MuxIntcP_enableOutEvent (int32_t muxNum, int32_t muxOutEvent) |
Function to enable interrupt controller mux for an output event. More... | |
void | MuxIntcP_disableOutEvent (int32_t muxNum, int32_t muxOutEvent) |
Function to disable interrupt controller mux for an output event. More... | |
Typedefs | |
typedef void(* | MuxIntcP_Fxn) (uintptr_t arg) |
Prototype for the entry function for a cpIntc interrupt. More... | |
typedef void(* | MuxIntcFxn) (uintptr_t arg) |
Prototype for the MuxIntc dispatch function. More... | |
Enumerations | |
enum | MuxIntcP_Status { MuxIntcP_OK = 0, MuxIntcP_FAILURE = (-(int32_t)1) } |
Status codes for MuxIntcP APIs. More... | |
Cross bar MuxNum definitions | |
#define | MUXINTCP_CROSSBAR_MUXNUM_DSP1 (0) |
#define | MUXINTCP_CROSSBAR_MUXNUM_DSP2 (1) |
#define | MUXINTCP_CROSSBAR_MUXNUM_IPU1 (2) |
#define | MUXINTCP_CROSSBAR_MUXNUM_IPU2 (3) |
#define | MUXINTCP_CROSSBAR_MUXNUM_MPU (4) |
#define | MUXINTCP_CROSSBAR_MUXNUM_INVALID (-(int32_t)1) |
#define MUXINTCP_CROSSBAR_MUXNUM_DSP1 (0) |
Cross bar MuxNum to be used for MuxIntcP_create()
#define MUXINTCP_CROSSBAR_MUXNUM_DSP2 (1) |
#define MUXINTCP_CROSSBAR_MUXNUM_IPU1 (2) |
#define MUXINTCP_CROSSBAR_MUXNUM_IPU2 (3) |
#define MUXINTCP_CROSSBAR_MUXNUM_MPU (4) |
#define MUXINTCP_CROSSBAR_MUXNUM_INVALID (-(int32_t)1) |
typedef void(* MuxIntcP_Fxn) (uintptr_t arg) |
Prototype for the entry function for a cpIntc interrupt.
typedef void(* MuxIntcFxn) (uintptr_t arg) |
Prototype for the MuxIntc dispatch function.
enum MuxIntcP_Status |
MuxIntcP_Status MuxIntcP_create | ( | MuxIntcP_inParams * | inParams, |
MuxIntcP_outParams * | outParams | ||
) |
Function to create an interrupt controller mux.
inParams | Pointer to the MuxIntcP input Parameters |
outParams | Pointer to the MuxIntcP output Parameters |
void MuxIntcP_enableInEvent | ( | int32_t | muxNum, |
int32_t | muxInEvent | ||
) |
Function to enable interrupt controller mux for an input event.
muxNum | Interrupt Controller mux number |
muxInEvent | Interrupt Controller mux input event ID |
void MuxIntcP_disableInEvent | ( | int32_t | muxNum, |
int32_t | muxInEvent | ||
) |
Function to disable interrupt controller mux for an input event.
muxNum | Interrupt Controller mux number |
muxInEvent | Interrupt Controller mux input event ID |
void MuxIntcP_clearInEvent | ( | int32_t | muxNum, |
int32_t | muxInEvent | ||
) |
Function to clear interrupt controller mux for an input event.
muxNum | Interrupt Controller mux number |
muxInEvent | Interrupt Controller mux input event ID |
void MuxIntcP_enableOutEvent | ( | int32_t | muxNum, |
int32_t | muxOutEvent | ||
) |
Function to enable interrupt controller mux for an output event.
muxNum | Interrupt Controller mux number |
muxOutEvent | Interrupt Controller mux output event ID |
void MuxIntcP_disableOutEvent | ( | int32_t | muxNum, |
int32_t | muxOutEvent | ||
) |
Function to disable interrupt controller mux for an output event.
muxNum | Interrupt Controller mux number |
muxOutEvent | Interrupt Controller mux output event ID |