2.2. Release Notes - 08_01_00¶
2.2.1. Introduction¶
This release notes provides important information that will assist you in using the PDK software package for the Jacinto family of devices. This document provides the product information and known issues that are specific to the PDK software package.
New features added / supported is listed below and defects fixed are highlighted in Fixed Issues. Also please check Upgrade and Compatibility for backward compatibility
2.2.2. What’s New¶
ID | Description | Module | Supported Platforms |
---|---|---|---|
JACINTOREQ-1168 | SDK shall support migration to LLVM/TI CLANG | COMMON | J721E, J7200, AM65XX |
PDK-9562 | IO Retention support Demo- GPIO | LPM | J7200 |
JACINTOREQ-1415 | PMIC LLD shall support GPIO Retention mode | PMIC | J7200 |
JACINTOREQ-1087 | PMIC LLD shall support LP8764x Hera PMIC | PMIC | J7200 |
JACINTOREQ-1416 | PMIC LLD shall support DDR Retention mode | PMIC | J721E, J7200 |
JACINTOREQ-1098 | PMIC LLD shall configure voltage, current, power good and thermal monitor | PMIC | J721E, J7200 |
JACINTOREQ-1090 | PMIC LLD shall support Watchdog in Trigger and Q&A Mode | PMIC | J721E, J7200 |
JACINTOREQ-1086 | PMIC LLD shall support TPS6594x Leo PMIC | PMIC | J721E, J7200 |
JACINTOREQ-1092 | PMIC LLD shall decipher error events and call out to application with error code | PMIC | J721E, J7200 |
JACINTOREQ-1097 | PMIC LLD shall support CRC | PMIC | J721E, J7200 |
JACINTOREQ-1088 | PMIC LLD shall support I2C and SPI communication interface | PMIC | J721E, J7200 |
JACINTOREQ-1104 | PMIC LLD shall support PFSM states | PMIC | J721E, J7200 |
JACINTOREQ-1094 | PMIC LLD shall support Low Power modes | PMIC | J721E, J7200 |
JACINTOREQ-1089 | PMIC LLD shall configure RTC for PMIC low power | PMIC | J721E, J7200 |
JACINTOREQ-1091 | PMIC LLD shall configure GPIO Pin Functionality | PMIC | J721E, J7200 |
JACINTOREQ-1093 | PMIC LLD shall configure BUCK and LDO regulator output voltages | PMIC | J721E, J7200 |
JACINTOREQ-1103 | PMIC LLD shall support ESM for MCU and SOC Errors | PMIC | J721E, J7200 |
JACINTOREQ-494 | Enet LLD: CPSW Inter clients (cores) packet communication | ENET | J721E, J7200 |
ETHFW-1711 | Enet LLD: Support MAC only mode of operation for few CPSW switch ports | ENET | J721E, J7200 |
2.2.3. Upgrade and Compatibility¶
2.2.3.1. FreeRTOS¶
- FreeRTOS is not supported on A72 core.
- FreeRTOS support is availble on all other cores. ( R5F )
- FreeRTOS Real-time Object View (ROV) in CCS IDE is available for R5F cores.
See FreeRTOS Chapter for more details.
2.2.3.2. TI-RTOS(SysBIOS)¶
- TI-RTOS(SysBIOS) is not supported on any cores from this release.
- RTOS support on A72 is also descoped.
2.2.3.3. NDK¶
- TI’s NDK TCP/IP stack is no longer supported on any cores.
- lwIP is now the only TCP/IP stack supported in this release.
2.2.3.4. OSAL¶
Following OSAL APIs which supported only TI-RTOS(SysBIOS) are descoped in this release.
- EventP
- EventP_pend()
- Migrate to similar API EventP_wait() which is supported for FreeRTOS
- QueueP
Descoped API Alternative API Osal_Queue_Handle QueueP_Handle Osal_Queue_Elem QueueP_Elem Osal_Queue_construct + Osal_Queue_handle QueueP_create Osal_Queue_put QueueP_put Osal_Queue_get QueueP_get Osal_Queue_empty QueueP_isEmpty
2.2.3.5. TI-CLANG¶
- This release introduces TI ARM Clang tool-chain/compiler for MCU R5 cores
- PDK drivers/examples are migrated from TI ARM CGT and validated with TI ARM Clang tool-chain.
- Note: TI ARM Clang tool chain generated code/binary size is more than that of TI ARM CGT.
See TI ARM CLANG Usage and Migration Guidelines Chapter for more details.
2.2.3.6. LPM¶
- LPM library provides a means on J7200 to move between Active mode and IO Retention mode.
- Scope would be to implement a Low Power Manager (LPM) running on MCU R5 core, with APIs to switch to and from IO Retention mode to ACTIVE mode on J7200 device with dual Leo + Hera PDN.
- When we come back from IO Retention to ACTIVE mode, programs can be executed on all other active cores.
- See LPM Chapter for more details.
2.2.4. Device Support¶
J7200 / DRA821 (BOARD=j7200_evm)
Associated TIFS versions:
TIFS name J721E SR revision tifs.bin SR1.0 GP tifs-hs-enc.bin SR1.0 HS
2.2.5. Validation Information¶
For details on the validated examples refer to the platform specific test report available here.
2.2.6. Tool Chain Information¶
Component | Version |
---|---|
FreeRTOS Kernel | 10.4.3 |
lwIP stack | 2.1.2 |
lwIP-contrib | 2.1.0 |
TI ARM CLANG | 1.3.0.LTS |
PRU code generation tools | 2.3.3 |
GCC ARM code generation tools | ARCH64 9.2-2019.12 |
CGT XML Processing Scripts | 2.61.00 |
System Analyzer (UIA Target) | 2_30_01_02 |
2.2.7. Change Request¶
ID | Head Line | Original Fix Version | New Fix Version |
---|---|---|---|
JACINTOREQ-1595 | PDK: XIP With OTFA Support Descope | 08.01.00 | None |
JACINTOREQ-2037 | PMIC Safety requirements needs to be moved to 8.2 release | 08.01.00 | 08.02.00 |
JACINTOREQ-1861 | SBL - Support to dump EEPROM is deferred to 8.2 release | 08.01.00 | 08.02.00 |
JACINTOREQ-1860 | SERDES sharing feature in SBL deferred to 8.2 release | 08.01.00 | 08.02.00 |
2.2.8. Fixed Issues¶
ID | Head Line | Module | Affected Versions | Affected Platforms |
---|---|---|---|---|
PDK-9490 | OSPI_Baremetal_Flash_Dma_TestApp fails on mpu1_0 in release mode | OSPI | 07.03.00 | J7200 |
ETHFW-1534 | [CPSW] Packet drop with QSGMII ports IPerf | ENET | 06.02.00 | J721E, J7200 |
ETHFW-1845 | examples: MAC loopback app test causes abort in debug mode during restart | ENET | 08.00.00 | J721E, J7200 |
PDK-10425 | Make for sbl_multicore_amp fails with proper last core of mpu1_1 | SBL | 08.00.00 | J721E, J7200, AM65xx |
PDK-10423 | IPC: RPMessage heap is sized wrong and is causing heap corruption of Rx messages | IPC | 08.00.00 | J721E, J7200, AM65xx |
2.2.9. Known Issues¶
ID | Head Line | Module | Reported in Release | Affected Platforms | Impact | Workaround in this release |
---|---|---|---|---|---|---|
PDK-6975 | Pulsar (R5F) : High priority interrupt is missed by VIM | CSL, OSAL | 07.00.00 | J721E, J7200, AM65xx | Baremetal implementation is pending | Use RTOS instead of baremetal |
PDK-9676 | UART : Potential interrupt storm | UART | 07.02.00 | J7200, J721E | Error interrupt resulting in hang. | None |
PDK-8601 | CSL ECC test application fails on J7200 | CSL | 07.01.00 | J7200 | None | None |
PDK-10128 | Spi_AsyncTransmit can not transmit more than 32 bytes | McSPI | 07.03.00 | J7200 | None | None |
PDK-10139 | J7200 App load on MCU R5_1 core may fail with CCS boot flow | COMMON | 08.00.00 | J7200 | Unable to run applications on MCU1_1 core through CCS/JTAG | None |
PDK-10925 | IPC Performance Test hangs after loading the binary | IPC | 08.01.00 | J721E, J7200, AM65xx | The app won’t work for this release | None |
PDK-10844 | Conflicting library definitions for __mpu_init() when using Clang compiler | CSL | 08.01.00 | J721E, J7200, AM65xx | User should link libraries in correct order | Ensure ti.csl.init.aer5f is the first library included and use –priority flag |
ETHFW-1904 | Enet: High packet drop in iperf UDP test | ENET | 08.01.00 | J721E, J7200, AM65xx | iperf UDP test will not run successfully | None |
2.2.10. Limitations¶
2.2.10.1. PDK¶
- PDK examples do not support SMP mode. Some of examples still support build in SMP mode but these binaries are not supported or validated.
- TI Clang compiler does not enable O3 optimization level and Thumb2 mode which were enabled by default with TI ARM CGT compiler. This has an impact on driver throughput. E.g. Ethernet performance has reduced by ~20% on J7200
- C++ build is not supported in this release for TI Clang compiler. It will be added back in next release.
2.2.10.2. ENET¶
- lwIP stack integration doesn’t support checksum hardware-offload feature.