PDK API Guide for J7200
|
DP83867 PHY configuration parameters.
Data Fields | |
bool | txClkShiftEn |
bool | rxClkShiftEn |
uint32_t | txDelayInPs |
uint32_t | rxDelayInPs |
uint8_t | txFifoDepth |
uint32_t | idleCntThresh |
uint32_t | impedanceInMilliOhms |
Dp83867_Gpio0Mode | gpio0Mode |
Dp83867_Gpio1Mode | gpio1Mode |
Dp83867_LedMode | ledMode [DP83867_LED_NUM] |
bool Dp83867_Cfg::txClkShiftEn |
Enable TX clock shift
bool Dp83867_Cfg::rxClkShiftEn |
Enable RX clock shift
uint32_t Dp83867_Cfg::txDelayInPs |
TX delay value
uint32_t Dp83867_Cfg::rxDelayInPs |
RX delay value
uint8_t Dp83867_Cfg::txFifoDepth |
TX FIFO depth
uint32_t Dp83867_Cfg::idleCntThresh |
Viterbi detector idle count threshold
uint32_t Dp83867_Cfg::impedanceInMilliOhms |
Output impedance in milli-ohms. Ranging from 35 to 70 ohms in steps of 1.129 ohms
Dp83867_Gpio0Mode Dp83867_Cfg::gpio0Mode |
Mux mode of the GPIO_0 pin
Dp83867_Gpio1Mode Dp83867_Cfg::gpio1Mode |
Mux mode of the GPIO_1 pin
Dp83867_LedMode Dp83867_Cfg::ledMode[DP83867_LED_NUM] |
LED mode (source) configuration