PDK API Guide for J7200
|
MAC port module configuration parameters.
Data Fields | |
bool | loopbackEn |
Enet_CrcType | crcType |
uint32_t | rxMtu |
bool | passPriorityTaggedUnchanged |
EnetPort_VlanCfg | vlanCfg |
EnetPort_EgressPriorityType | txPriorityType |
EnetMac_SgmiiMode | sgmiiMode |
bool CpswMacPort_Cfg::loopbackEn |
Whether loopback mode is enabled or not
Enet_CrcType CpswMacPort_Cfg::crcType |
Type of CRC
uint32_t CpswMacPort_Cfg::rxMtu |
Max length of a received frame on ingress. This max length includes VLAN
bool CpswMacPort_Cfg::passPriorityTaggedUnchanged |
Whether priority tagged packets should be passed unchanged (if set to true) or replaced with port's VID (if set to false)
EnetPort_VlanCfg CpswMacPort_Cfg::vlanCfg |
Port VLAN configuration
EnetPort_EgressPriorityType CpswMacPort_Cfg::txPriorityType |
Egress priority type
EnetMac_SgmiiMode CpswMacPort_Cfg::sgmiiMode |
SGMII mode. Applicable only when port is used in Q/SGMII mode