PDK API Guide for J7200
|
Multicast entry type info apart from MAC address.
Data Fields | |
bool | super |
CpswAle_FwdStateLevel | fwdState |
uint32_t | portMask |
uint32_t | numIgnBits |
bool CpswAle_McastEntryInfo::super |
Supervisory flag which indicates that this address can be received in port state other than Forwarding state
CpswAle_FwdStateLevel CpswAle_McastEntryInfo::fwdState |
Forward state level
uint32_t CpswAle_McastEntryInfo::portMask |
Port bit mask that is returned with a found multicast destination address
uint32_t CpswAle_McastEntryInfo::numIgnBits |
Number of bits in the address to ignore. Up to 10 least significant bits can be ignored to form a multicast address range