ETHFW API Guide
|
Register IPv4:MAC Address mapping CMD request params.
Data Fields | |
struct rpmsg_kdrv_ethswitch_message_header | header |
struct rpmsg_kdrv_ethswitch_common_request_info | info |
uint8_t | mac_address [RPMSG_KDRV_TP_ETHSWITCH_MACADDRLEN] |
uint8_t | ipv4_addr [RPMSG_KDRV_TP_ETHSWITCH_IPV4ADDRLEN] |
struct rpmsg_kdrv_ethswitch_message_header rpmsg_kdrv_ethswitch_ipv4_register_mac_request::header |
Common CMD header
struct rpmsg_kdrv_ethswitch_common_request_info rpmsg_kdrv_ethswitch_ipv4_register_mac_request::info |
Common info associated with all CMDs other than ATTACH
uint8_t rpmsg_kdrv_ethswitch_ipv4_register_mac_request::mac_address[RPMSG_KDRV_TP_ETHSWITCH_MACADDRLEN] |
Mac address associated with the IP address which should be added to the ARP table
uint8_t rpmsg_kdrv_ethswitch_ipv4_register_mac_request::ipv4_addr[RPMSG_KDRV_TP_ETHSWITCH_IPV4ADDRLEN] |
IPv4 address