![]() |
PDK API Guide for J7200
|
Icssg TX timestamp event callback info structure. This is passed to application when TX timestamp is retrieved by ICSSG driver.
Data Fields | |
uint32_t | txTsId |
uint64_t | ts |
uint32_t Icssg_TxTsEvtCbInfo::txTsId |
Timestamp Id. This was passed by an application when enabling the timestamp for the packet during EnetDma_submitTxPktQ()
uint64_t Icssg_TxTsEvtCbInfo::ts |
Packet timestamp