Files | |
| file | TaskP.h |
| Task module for the RTOS Porting Interface. | |
Data Structures | |
| struct | TaskP_Params |
| Basic TaskP Parameters. More... | |
Macros | |
| #define | OS_TICKS_IN_MILLI_SEC 1 /* 1000us tick */ |
| Number Ticks by OS in 1 millisecond. More... | |
Typedefs | |
| typedef void * | TaskP_Handle |
| Opaque client reference to an instance of a TaskP. More... | |
| typedef unsigned long | TaskP_Privilege_Mode |
| [SafeRTOS only] Privilege of the task in safertos More... | |
| typedef void(* | TaskP_Fxn) (void *arg0, void *arg1) |
| Prototype for TaskP function. More... | |
Enumerations | |
| enum | TaskP_Status { TaskP_OK = 0 , TaskP_FAILURE = (-(int32_t)1) } |
| Status codes for TaskP APIs. More... | |
Functions | |
| TaskP_Handle | TaskP_create (TaskP_Fxn taskfxn, const TaskP_Params *params) |
| Function to create a task. More... | |
| TaskP_Status | TaskP_delete (TaskP_Handle *handle) |
| Function to delete a task. More... | |
| void | TaskP_Params_init (TaskP_Params *params) |
| Initialize params structure to default values. More... | |
| void | TaskP_sleep (uint32_t timeout) |
| Function for Task sleep in units of OS tick. More... | |
| void | TaskP_sleepInMsecs (uint32_t timeoutInMsecs) |
| Function for Task sleep in units of msecs. More... | |
| void | TaskP_setPrio (TaskP_Handle handle, uint32_t priority) |
| Function to update Task priority. More... | |
| TaskP_Handle | TaskP_self (void) |
| Function returns the Task handle of current task. More... | |
| TaskP_Handle | TaskP_selfmacro (void) |
| Function returns the Task handle of current task.This is an inline function. More... | |
| void | TaskP_yield (void) |
| Function Yield processor to equal priority task. More... | |
| uint32_t | TaskP_isTerminated (TaskP_Handle handle) |
| Check if task is terminated. More... | |
| uint32_t | TaskP_disable (void) |
| Disable the task scheduler. More... | |
| void | TaskP_restore (uint32_t key) |
| Restore Task scheduling state. More... | |
| uint32_t | TaskP_getTaskStackHighWatermark (TaskP_Handle handle) |
| Return the task stack high watermark value (in bytes) More... | |
Variables | |
| const char * | TaskP_Params::name |
| int8_t | TaskP_Params::priority |
| uint8_t | TaskP_Params::padding1 |
| uint16_t | TaskP_Params::padding2 |
| uint32_t | TaskP_Params::stacksize |
| void * | TaskP_Params::pErrBlk |
| void * | TaskP_Params::arg0 |
| void * | TaskP_Params::arg1 |
| void * | TaskP_Params::stack |
| void * | TaskP_Params::userData |
| TaskP_Privilege_Mode | TaskP_Params::taskPrivilege |
TaskP interface
| #define OS_TICKS_IN_MILLI_SEC 1 /* 1000us tick */ |
Number Ticks by OS in 1 millisecond.
| typedef void* TaskP_Handle |
Opaque client reference to an instance of a TaskP.
A TaskP_Handle returned from the TaskP_create represents that instance and is used in the other instance based functions
| typedef unsigned long TaskP_Privilege_Mode |
[SafeRTOS only] Privilege of the task in safertos
A TaskP_Privilege_Mode can have two values as below. mpuUNPRIVILEGED_TASK value is 0. mpuPRIVILEGED_TASK value is 1.
| typedef void( * TaskP_Fxn) (void *arg0, void *arg1) |
Prototype for TaskP function.
| enum TaskP_Status |
| TaskP_Handle TaskP_create | ( | TaskP_Fxn | taskfxn, |
| const TaskP_Params * | params | ||
| ) |
Function to create a task.
| taskfxn | Function pointer of the task. |
| params | Pointer to the instance configuration parameters. |
| TaskP_Status TaskP_delete | ( | TaskP_Handle * | handle | ) |
Function to delete a task.
| handle | A TaskP_Handle returned from TaskP_create |
| void TaskP_Params_init | ( | TaskP_Params * | params | ) |
Initialize params structure to default values.
| params | Pointer to the instance configuration parameters. |
| void TaskP_sleep | ( | uint32_t | timeout | ) |
Function for Task sleep in units of OS tick.
| timeout | sleep ticks. |
| void TaskP_sleepInMsecs | ( | uint32_t | timeoutInMsecs | ) |
Function for Task sleep in units of msecs.
| timeoutInMsecs | sleep in units of msecs. |
| void TaskP_setPrio | ( | TaskP_Handle | handle, |
| uint32_t | priority | ||
| ) |
Function to update Task priority.
| handle | A TaskP_Handle returned from TaskP_create. |
| priority | New priority to be set. |
| TaskP_Handle TaskP_self | ( | void | ) |
Function returns the Task handle of current task.
| TaskP_Handle TaskP_selfmacro | ( | void | ) |
Function returns the Task handle of current task.This is an inline function.
| void TaskP_yield | ( | void | ) |
Function Yield processor to equal priority task.
| uint32_t TaskP_isTerminated | ( | TaskP_Handle | handle | ) |
Check if task is terminated.
Typically a task MUST be terminated before it can be deleted.
| uint32_t TaskP_disable | ( | void | ) |
Disable the task scheduler.
Control Task scheduling. This disables all other Tasks from running until TaskP_restore is called. Interrupts can still run.
| void TaskP_restore | ( | uint32_t | key | ) |
Restore Task scheduling state.
Resumes the scheduler after it was disabled using a call to TaskP_disable.
| key | key to restore previous Task scheduler state |
| uint32_t TaskP_getTaskStackHighWatermark | ( | TaskP_Handle | handle | ) |
Return the task stack high watermark value (in bytes)
This represents the smallest distance in bytes thus far before experiencing a stack overflow
| handle | A TaskP_Handle returned from TaskP_create. |
| const char* TaskP_Params::name |
Name of the task instance.
| int8_t TaskP_Params::priority |
The priority of the task
| uint8_t TaskP_Params::padding1 |
Padding for structure alignment
| uint16_t TaskP_Params::padding2 |
Padding for structure alignment
| uint32_t TaskP_Params::stacksize |
The stack size of the task
| void* TaskP_Params::pErrBlk |
Pointer to the error block for task Create
| void* TaskP_Params::arg0 |
argument 0
| void* TaskP_Params::arg1 |
argument 1
| void* TaskP_Params::stack |
pointer to stack memory, shall be non-null value
| void* TaskP_Params::userData |
[SafeRTOS, FreeRTOS only] Pointer to user-defined data
| TaskP_Privilege_Mode TaskP_Params::taskPrivilege |
[SafeRTOS only] Privilege mode of the task